| FA169761 | What does ‘Integr Inst’ means when looking at the trip history on a micrologic P.
The message ‘ Integr Inst' means a tripping by the instantaneous self-protection built into the device that is called as DIN/DINF.
When such message... |
| FA169760 | Is there any temperature derating table available for Compact NSX DC PV circuit breaker. The temperature derating table for Compact NSX DC PV circuit breaker is attached below. |
| FA169759 | What is the maximum rated operational voltage (Ue) of Compact NSX DC PV MCCB. The maximum rated operational voltage of Compact NSX DC PV MCCB is 1000 VDC. |
| FA169758 | Is it required to remove the rating plug in Micrologic E of Masterpact NW/NT & Compact NS 630b … 1600 A circuit breakers while performing megger test. The Micrologic E has a different technology than that of Micrologic A, P and H.
The Micrologic E measures the voltage through a high impedance... |
| FA169757 | Is there any tripping curves available for Compact NSX DC PV circuit breaker. The tripping curves for Compact NSX DC PV MCCB are available and are attached below.
|
| FA169756 | Does the Modbus Chassis Communication Module (CCM) support 2 wire RS485 communications. The Modbus Chassis Communications Module does support 2 wire RS485 communications.
The module can be configured by jumpering the IN+ and the OUT+... |
| FA169755 | What is the default baud rate , address and parity of Breaker Communications Module (BCM) and Chassis Communications Module (CCM). For the CCM the Default values are: Baud rate = 19.2 K , Address = 97, Parity = even
For the BCM the default values are: Baud rate = 19.2 K, Address... |
| FA169754 | What is the limit on Modbus multi drop connection for both the HMI port and also on the Modbus port in TeSys T. The limit on the left or the right port for TeSys T Modbus product is the same.
These features are defined by Modbus standard: maximum 1000 meters... |
| FA169752 | Is there any dual redundancy available with TeSys T’s offer. Yes, it is available with Ethernet Product only. This is the dual port technology which allows that.
The redundancy is for Ethernet Communication... |
| FA169751 | Is it possible to feed the supply from top (upstream) and bottom (downstream) in compact NSX range MCCB. Compact NSX circuit breakers can be supplied from either the top or the bottom, even when equipped with a Vigi
earth-leakage protection module, without... |