| FA167666 | How Ecodial Advance Calculation, determines the "type of LV capacitor banks”? The type of capacitor bank is determined by calculating the Gh/Sn ratio, which is the total harmonic disturbance level of the installation: |
| FA167663 | How Ecodial Advance Calculation, determines the "type of regulation" of "LV capacitor banks”? According to the following rules; Ecodial Advance Calculation proposes the type of regulation (fixed or automatic) of capacitor banks:
- If the power... |
| FA167669 | In Ecodial Advance Calculation, what do you mean by "phase balancing"?
As shown above the network is ‘drawn', and the connected loads are defined as “10Amps single phase loads”…then we can see that “all these single... |
| FA167645 | Why Ecodial Advance Calculation proposes the 'limited discrimination', for some combination of protection devices, where the same in complementary technical information says "total discrimination"?
In complementary technical information;
While seeing the combination of upstream & downstream devices (Example: see the above table) the magnetic... |
| FA167644 | In Ecodial Advance Calculation, will it possible to make discrimination as optional for the protection selection? No, In Ecodial Advance Calculation – the discrimination constraint is not optional for the protection device selection.
In other words: Ecodial Advance... |
| FA167641 | In Ecodial Advance Calculation, where is the function "Decor?" In Ecodial Advance Calculation, We don’t have the function – Decor.
Which was present in My Ecodial L, and helps the user to Decorate around the schematic
In... |
| FA167639 | In Ecodial Advance Calculation, Where is function standard diagram? In Ecodial Advance Calculation, We don’t have the function – Standard Diagram.
Which was present in My Ecodial L, and It was used to quickly access... |
| FA167638 | In Ecodial Advance Calculation, why the 'number and type of conductor' is always "undefined" for the Feeder circuit? In Ecodial Advance Calculation, value for this parameter ‘number and type of conductor’ will be propagated from down-to-top basis.
At the switchboard... |
| FA167636 | In Ecodial Advance Calculation, why the 'type of system earthing' is always "undefined" for the Feeder circuit? In Ecodial Advance Calculation, value for this parameter ‘Type of system earthing’ will be propagated from top-to-down basis.
Yes, we can also see... |
| FA167634 | In Ecodial Advance Calculation, will it possible to define the 'general information' of project? Yes, In Ecodial Advance Calculation the ‘general information’ of the project cab be defined. Then this can also be printed & given along with the... |