| FA166342 | What are the different types of Encoder interface cards available & how to install in Altivar 71 drive. Refer to attached file for different types of Encoder interface cards
available & how to install in Altivar 71 drive. |
| FA166337 | What is the Pin out of the Altivar 312 RJ45 Connector. Refer to attached file for the Pin out of the Altivar 312 RJ45 Connector. |
| FA166336 | How to connect Altistart 48 Soft Starter to “connection to delta in the motor”. Refer to attached file for “connection to delta in the motor”.
|
| FA166305 | What accessory is needed to connect the two reels of RG11 trunk cable. Ground Blocks is to be used while connecting two reels of RG11 trunk cable.
The 60-0545-000 Ground Block consists of two female in-line F connectors... |
| FA166231 | What is the difference difference in the communication cable TWDXCARJXXX and TSXCRJMD25 used for Twido modbus connection on Port1. Both the cables are for different purpose.
TWDXCARJXXX cable is being used for the serial modbus communication where DPT signal of pin 5 is being... |
| FA166230 | What is the error 8130h means in Advantys Island which consist STB NIP2311 and some digital Input and Output modules.
The error 8130h on an Advantys island generally comes when there is Loss of fieldbus communication, NIM
communication error or internal bus error.
To... |
| FA143570 | Does the Advantys Configuration Software STBSPU1000 include a programming cable. Yes, the Advantys Configuration Software STBSPU1000 comes with a STBXCA4002 programming cable to connect the
NIM to the PC. The cable length is 2... |
| FA149725 | What is the usage of TSXPACC01 in unitelway communication. The TSXPACC01 unit is a cabling accessory that connects to the TER connector of the Premium/Atrium PLC processor via
an integral cable fitted with... |
| FA149723 | What are the Pin outs for TSXCUSB232 for serial port as well as USB port.
Please find attached the instruction sheet as below.
|
| FA138274 | How to connect terminal box TSXPACC01 to TSX Micro controllers. Refer to attached Instruction manual for illustration of Terminal box TSXPACC01 connection to
Modicon TSX Micro controllers. |