Narrow By
  1. Your SelectionAll

Cabling and Connection - FAQs

FAQ Search
Most Recently Published FAQs

Results 21 - 30 of 100

FAQ ID Description
FA143568What is the part number for the fiber cable used between the Primary and Standby CPU's in a Unity Hot Standby application, Is this cable included in my purchase of the HSBY processor.
This cable is not included in your purchase of the 140CPU671 60. The part number(s) of the fiber MT/RJ cable are, 490NOR0003      3 m MTRJ/ MTRJ 490NOR0005     ...
FA135501How to troubleshoot the communication issues between Laptop and Programmable logic controller(Twido/TSX Micro/Premium) using TSXCUSB485 cable.
It is possible to use TSXCUSB485 + TSXCRJMD25 Programming cable to upload application program from programmable logic controller (PLC) to Laptop/Computer...
FA137292How to connect an Encoder to Twido Controller.
Refer to attached document for Wiring diagram between Twido and an Encoder.
FA136534Provide the communication port details of Twido Controllers.
All Twido Controllers have inbuilt 8-pin MiniDIN RS485 Port1 and other optional Port2 based on part numbers have to ordered separately and refer...
FA21083What is the insulation voltage rating for cables BMX FTW and BMX FCW in Modicon M340 range.
The dielectric withstanding (VDC) for cables BMX FTW and BMX FCW is 1000 Volts applied for 1 minute and th minimum specific insulation resistance...
FA134927What are the minimum and maximum wires sizes required for the M340 Power Supply connectors.
The wire size for the 5-pin screw terminal block delivered with the module is  24-12 AWG.
FA86526How to connect the Remote Display (HMI) Unit of Altivar 71 via LU9GC3 Modbus splitter
The Remote Display (HMI) unit of the Altivar 71/ 61 drive takes it power from the drive port to which it is connected. When the same Remote Unit...
FA22920Why and when should I use a line choke upstream from an ATV31,ATV312, ATV61, ATV71 variable speed drive?
A line choke is used to provide better protection against overvoltages on the line supply and to reduce the harmonic distortion of the current produced...
FA23075Can I install a potentiometer, part number SZ1RV1202, in an XACA enclosure?
No. There are two reasons preventing a potentiometer, part number SZ1RV1202, from being installed in an XACA enclosure: 1. An SZ1RV1202 potentiometer...
FA23735Where should I connect the SZ1RV1202 potentiometer (pot) to the ATV variable speed drives?
The potentiometer part number: SZ1RV1202 must be connected to one of the 0...10 V analog inputs on ATVxxxx range variable speed drives: ATV12...

Results 21 - 30 of 100