Narrow By
  1. Your SelectionAll

Firmware and Drivers - FAQs

FAQ Search
Most Recently Published FAQs

Results 11 - 20 of 40

FAQ ID Description
FA21086How to calculate the scan time of Hot Stand-By (HSBY) system in Modicon Quantum range.
Considering the Hot Stand-By system, the scan time mainly comes from the addition of three parts:   Part 1: User application logic execution time,...
FA12093What are the different part references for the programming software and communication cable to be used for Modicon Micro Range PLCs.
There are three different PL7 software packages that can be used for programming of the Modicon Micro Range of PLCs. 1. TLXCDPL7PP45M.....PL7 PRO...
FA86522Which version of Web Designer software is compatible with M340 NOR Module (RTU) Firmware version 1.0
The Web Designer V2.23 is compatible with the M340 NOR Module (RTU) Firmware version 1.0 and should be used for designing the webpages.
FA86519Which version of Web Designer software is compatible with M340 NOE Module (Ethernet) Firmware version 4.5 and 4.6
The Web Designer V2.22 is compatible with the M340 NOE Module (Ethernet) Firmware version 4.5 and 4.6 and should be used for designing the webpages.
FA21080Why does the compatibility check error come while downloading Unity Pro V4.0 application to Modicon M340 PLC.
The error appears due to incompatibility between Unity Pro V4.0 and firmware version of the M340 CPU. Unity Pro V4.0 application is compatible with...
FA86513What are the built-in RTU Protocol and Function available in M340 -Unity Pro 5.0 Platform
M340 offers two module references for RTU. 1.) BMX NOR 0200 (for normal environment) 2.) BMX NOR 0200H (for Harsh environment)   RTU communications...
FA86515What is the version compatibility for M340 NOE Module (Ethernet) and Processor
The following table shows compatible combinations for M340 NOE Module and M340 Processor: * In this case the NOE module will not be reconized as...
FA149724Can I have driver for TSXCUSB232 and TSXCUSB485, while installing in Windows 7 (Win7).
Please find attached the drivers as below.
FA22665Is it possible to read the IP address of connected device at runtime in Vijeo Designer.
Yes, it is possible to read the IP address of connected devices via scripting during runtime. This feature has been implemented in Vijeo Designer...
FA22664Is it possible to write a new IP address of connected device at runtime in Vijeo Designer.
Yes, it is possible to write a new IP address of connected devices via scripting during runtime. This feature has been implemented in Vijeo Designer...

Results 11 - 20 of 40