| FA146152 | How to upgrade the firmware of ATV-IMC without using SoMachine. Find attached the description of a tool which allows the user to upload the ATV-IMC firmware in a very simple way, without the use of SoMachine. |
| FA145752 | What is the minimum software version for Altivar 61 drive that is compatible with the IMC controller card VW3A3521. The ATV IMC is compatible with Altivar 61 drive software version V2.1IE23 and upper versions. |
| FA141466 | How to upgrade firmware version of M238 Controller. Refer to attached file for procedure to upgrade the firmware version of Modicon M238 Controller. |
| FA159968 | Where to find Zelio USB Driver for cable SR2USB01. The USB Driver for Programming Cable SR2USB01 is included inside the ZelioSoft2 Programming Software SR2SFT01.
Find attached the USB Driver for Programming... |
| FA164052 | How to update the firmware of the TCSESM Ethernet Managed Switches. Follow the procedure to update the firmware of the Ethernet managed switch.
1. Open the webpage by typing the IP address of the Switch.
2. Go to... |
| FA161908 | Is it possible to update the firmware of the Altistart 48 control board (VX4G481). The best way is to order and replace the new control board with the latest version.
It is not possible to update the firmware of Altistart 48 because... |
| FA11929 | How to install the USB driver for Zelio Soft2 and install USB cable SR2USB01. Follow the step by step procedure in order to install the USB driver for Zelio Soft2 and the USB cable SR2USB01 for two different operating systems... |
| FA11801 | How to access program inside Zelio Logic when password is forgotten. In case the user has lost or has forgotten the program password, there is no way to access the program inside Zelio logic.The only solution is overwriting... |
| FA12091 | What does the Counters 22, 2C, 2E, 2F depict in FIPIO Communication. Counter 2Eh (Number of Pierced Frame Fault): This counter allows diagnoses of the receipt of a silent inside a frame i.e. between the identification... |
| FA12161 | What is the minimum Power suite software version required for Bluetooth Adapter on Altivar 31. The minimum Power Suite version for using the Bluetooth feature with Altivar 31 Drive is V2.2.The part reference for the Bluetooth adapter is VW3A8114. The... |