Hardware Compatibility - FAQs

FAQ Search
Most Recently Published FAQs

Results 31 - 40 of 83

FAQ ID Description
FA142349Do we have any retrofit accessory that converts extended rotary handle GV2AP01 to GV2APN01.
The GV2APN01 is the extended rotary handle for GV2P/L series of MPCB. The GVAPP1 is the retrofit accessory that converts GV2AP01 to GV2APN01.
FA12216What is the maximum number of sensors and resistance values which can be connected to the T1 and T2 terminals on TeSys T.
You can wire maximum 6 sensors (PTC or NTC analog) to Temperature Input terminals T1 and T2 on TeSys T.And, you can go up to a maximum of 6500 ohms...
FA12215Can TeSys T be used downstream of Altivar range Variable Speed Drive.
The Current Transformers (CTs) of TeSys T are deigned to work under the frequency range between 47 to 63 Hz only. However, the output frequency range...
FA12192Is it possible to control the motor from TeSys T via the PowerSuite software.
The configuration of TeSys T, read diagnostic, parameter setting and custom logic development is possible via PowerSuite software.However, the controls...
FA12191Is it possible to connect the different control voltages at the input of LTMR module in TeSys T.
Control Voltage characteristics You can connect different control voltages on the input of the LTMR TeSys T module, if the voltage and current ratings...
FA12193What is the maximum current which can be measured by TeSys T.
810 A is the maximum current that can be measured by the TeSys T as per the Schneider Electric offer catalogue.However, as per the TeSys T hardware/software...
FA12196Can TeSys T be used for Single Phase application.
Yes, TeSys T can be used in Single Phase application.  For a Single Phase application, you pass the First Phase cable through the first internal CT...
FA12190Is it possible to use LTME DC Expansion module with LTMR AC module of TeSys T.
Yes, it is possible to use LTME DC Expansion module with LTMR AC module of TeSys T.
FA12186Is it possible to do remote reset function with ASI module ASILUF05 of TeSys U.
ASILUFC5 unit works on the ASI bus which is a basic bus and handles only 31 or 62 slaves. This unit cannot support the remote reset function alone.The...
FA164056140 NOC 771 •• module supported in Hot standby configuration.
140 NOC 771 •• module is supported only in standalone systems; the module is not supported in Hot Standby system/configuration.

Results 31 - 40 of 83