| FA22774 | What are the characteristics of STR13MAE (MAE500) trip unit used in Compact NS630 circuit breaker. The Compact NS630 fitted with the STR13MAE trip unit is named: NS630MAE500.
The old MA500 trip unit was designed with mechanical feature. The new... |
| FA12107 | How the mechanical interlocking can be done between Masterpact M and Masterpact NW ACB’s by using two interlocks and one key. To interlock the two Air Circuit Breakers (ACBs) with the same key, you need to order the Ronis keylock reference 48550 or Profalux keylock 48546.For... |
| FA12079 | What are the Spare Reference Numbers of Finger Contacts and Arms of LF2 (SF6 Breaker). The spare reference number of Finger Contacts of LF2 (SF6 Breaker) is AAV48765. A single kit contains 6 sets of Finger clusters.However, the Arm is... |
| FA12086 | What are the recommended Cable Sizes and the Tightening Torque values for the Multi9 Final Low Voltage (FLV) range of products. The recommended Cable Sizes and the Tightening Torque values for the Multi9 Final Low Voltage (FLV) range of products is given in the attached document.... |
| FA22773 | What are the available part references to provide the different key locks with same keys in Compact NS. To order a quantity of several locks with same set of keys, refer the table given below :
Sr. No.
Identical... |
| FA22770 | Is the installation of 31097 locking kit same as the 31088 in Interpact source changeover system. Yes, the installation of the 31097 & 31088 locking kits is the same, as all key locks have been designed to achieve locking in the OFF position.
Refer... |
| FA12201 | Is it possible to order the Finger Contacts and Arms of LF2 breaker separately. The Finger contacts can be ordered separately. Reference for the Finger Contacts Kit for LF2 Breaker is AAV48765. The kit contains 6 sets of Finger... |
| FA11552 | How to use RCCB-ID in Three Phase Network. RCCB-ID can be used for Three Phase Network (220/440V AC).Refer attachment for the connection of RCCB-ID in 3 Phase (220/440V AC) network. |
| FA22775 | How many UA150 ATS controller can be used with one DC150 module. Only one UA150 controller can be used per DC150 and its Digipact address must be set at 14-14. |
| FA12101 | What are the minimum and maximum cable sizes recommended for use with TeSys D Star-Delta connection kits. The minimum and maximum cable sizes recommended to be used with TeSys D Star-Delta kits are: Kit Minimum (Sq. mm)... |