Narrow By
  1. Your SelectionRemove All

Other - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA277647Is it possible to transform compact NSX NA switch disconnector into circuit breaker by changing trip unit.
Compact NSX NA switch disconnectors cannot be transformed into circuit breakers by changing trip unit, this solution has not been validated by Schneider. ...
FA277652Is it possible to order NSX NA trip unit separately.
It is not possible to order separately the NSX NA trip units  
FA21081What is the reference number for the Modbus Plus Tap Spare plastic caps.?
The little plastic caps come along with the Modbus Plus Tap and they cannot be ordered separately.  
FA27988Can I replace a broken toggle on an NS / NSX circuit-breaker or switch.?
No, the toggle on the breaker frame cannot be replaced as the toggle is integral to the breaker frame. The breaker frame needs to be replaced. However,...
FA22583What is the full name of the abbreviation 'STR' trip unit ? .
 The abbreviation 'STR' has a very old origin. The first generations of trip units were called Statimax and 'STR' refers to "Statimax Trip Release".
FA27969How can I obtain the manufacturing date of the Compact NS or NSX circuit-breakers ?
To obtain the manufacturing date of Compact NS or NSX circuit-breakers, read the screen-printed marking at the top of the front panel. The code P07351,...
FA23075Can I install a potentiometer, part number SZ1RV1202, in an XACA enclosure?
No. There are two reasons preventing a potentiometer, part number SZ1RV1202, from being installed in an XACA enclosure: 1. An SZ1RV1202 potentiometer...
FA256219What is EEF1 fault on Altivar 71 drive.
EEF1 is a control EEprom Fault and at starting, the microprocessor on the application board tries to read and write to the EEPROM. If it is impossible,...
FA256218Is push button & receiver of wireless and batteryless package XB5RMA04 comes as factory-paired.
If you order XB5RMA04 pack, then following item comes on this pack and it is already factory-paired: -----  (1) => 1 number wireless and battery less...
FA255317For the setting of the PTC probe in the fault management, if we set it to Motor On, will the sensing of the LI6 happen when the Altivar 71 drive sends run command to motor.
If you set PtCL to [Motor ON], then it will monitor the resistance Value when the VSD sends a run command to motor. For information: Input for a...

Results 1 - 10 of 100