Options and Accessories - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA285686What are the reference of SFP Socket required for M580 HSBY sync link and its speed.
●A selectable SFP socket are Available: ●490 NAC 0100 - RJ45 (max. length = 100m) ●490 NAC 0201 - Fiber Optic LC Single Mode (max. length = 15km)   ●The...
FA285683Do we have pre-wired Cable arm for Quantum IO modules.
Yes, we are having the pre-wired cable cordset for Quantum IO modules. Refer the attached document for the selection of pre-wired cordset and respective...
FA276099What is the part number of remote mounting kit for the ATV Process Drive keypad?
Issue: What is the part number of remote mounting kit for the ATV Process Drive keypad? Product line: ATV Process, Altivar 630, ATV630 Environment: All Cause: Customer...
FA283624What is the part number for the fan cover for the ATS46 softstarter?
Issue: Fan Cover part number Environment: Replacement parts Cause: Fan cover replacement. Resolution: See attached document for fan cover part numbers....
FA283625What is the part number for the ATS46 Fan thermal switch?
Issue:Fan thermal switch part number Environment: Replacement parts Cause: Fan thermal switch failure. Resolution: See attached document for fan thermal...
FA284604For how much time CPU backup will be retained if both power and battery is not available with TSXPSY2600.
The backup time depends on the ambient temperature. Assuming that the processor was switched on previously, the typical backup time varies in the...
FA283626What is the part number for the firing board for a ATS46 softstarter?
Issue: Firing board part number Environment: Replacement parts Cause: Firing board failure. Resolution: See attached document for the firing board...
FA31962When the C60H & iC60H circuit breaker are locked ON with the padlocking facility, will it still trip under fault conditions ?
Yes, all of the miniature circuit breakers have a "trip free" mechanism which enables them to trip under fault conditions even if the handle is locked...
FA31963If the C120H circuit breaker is locked ON with the 27145 padlocking facility will it still trip under fault conditions?
Yes, all of the miniature circuit breakers have a "trip free" mechanism which enables them to trip under fault conditions even if the handle is locked...
FA278974What is the part number for the Battery Temp Sensor (BTS) for my Xantrex or Solar product?
Issue: Customer is searching for a replacement part number for a BTS. Product Line: Conext XW+, Conext XW, Conext SW, Trace Inverters, Legacy Products Environment: All...

Results 1 - 10 of 100