| FA22893 | What are the differences between the various tripping classes of thermal overload? There are four classes of thermal overload relay:
10A
10
20
30
These class numbers indicate the trip characteristics from cold state, and should be... |
| FA22848 | Are the heads of XY2CDxx trip-wire switches available separately? Yes, the head for XY2CDxx trip-wire switches can be ordered as a spare part, number XY2CD01 |
| FA22740 | Is there an additional light diffuser available for XVB and XVD illuminated Tower Beacons Yes, the light diffuser, part number XVBZ18 (consisting of two half-cylinders) can be placed in the illuminated lens unit so as to create a new light... |
| FA22734 | What is the maximum number of units that can be assembled on an XVP beacon tower? It is possible to stack a combination of up to 5 illuminated and audible units (one audible unit maximum) to create an XVP beacon tower.
Example... |
| FA22706 | What is the part number of the Harmony Padlockable Flaps? It is ZB4BZ6x, to which the number corresponding to the colour must be added: 2 = Black 4 = Red 5 = Yellow 6 = Blue
|
| FA22661 | Can the OA1 output of Tesys U be used with multifunction unit to drive a separate motor contactor. Output OA1 for Tesys U with base contactor (LUB**) is only used to drive the contactor embedded inside the TesysU contactor base LUB.
In order to use... |
| FA22659 | Can the same mechanical interlock for LC1FL44 contactor be used for mechanical interlock of the new equivalent LC1F6304 contactor. Yes, the same mechanical interlock LA9FL970 can be used for both the old LC1FL44 as well as for new equivalent LC1F6304 contactors. This is a horizontally... |
| FA22653 | Is it possible to use the current Limiter LA9LB920 or GV1L3 with Tesys GV3 range of MPCB to increase the breaking capacity. LA9LB920 and GV1L3 current limiter are dedicated to Tesys GV2 Motor Protection Circuit Breaker (MPCB) product range and can be used with MPCB rated... |
| FA142347 | Do we have spare set of contacts and arc chambers available for Tesys D range of contactors. The spare set of contacts and arc chambers are only available for Tesys 115 & 150 A contactors.
Refer the below screen-shot for the details
|
| FA137933 | How is the Harmony XB5S Biometric Switch mounted. The Harmony XB5S biometric switch can be mounted in a standard hole for a 22 mm push button.
It can be connected with simple wires or an M12 connector.... |