| FA12219 | How to mount the Rectifier DR5TE on TeSys F range of contactor. The DR5TE4U rectifier is mounted separately off the coil on a little support sold with the coil. Refer attachment for the mounting instruction of... |
| FA12214 | What is the maximum length of the connector cable between the LTMR and LTME module in TeSys T Range. Three different length connectors are available for connecting the LTMR and LTME module.The maximum length between the connections of TeSys T controller... |
| FA12194 | What is the short circuit current rating for TeSys GV2G Comb Busbar. The short-circuit current withstand rating (KA) of Tesys Comb Busbar is compatible with the breaking capacity of Motor Protection Circuit Breakers... |
| FA12113 | What are the various parts included in the LA91217 Star Delta connection kit. The different parts contained in the LA91217 Star Delta connection kit is as shown in the below figure. |
| FA22849 | Can I purchase separately the contact block or the rotary head of a ZCKJxx limit switch? We cannot supply either the contact block or the rotary head of the ZCKJxx body separately, because the actuation angle of the head is set by adjusting... |
| FA162153 | What is the function and ordering part number for the Cradle Communication Module (CCM). Part reference of Cradle Communication Module (CCM) is 33110.
Function of CCM: - The CCM is independent from the Chassis so when the ACB inside... |
| FA162152 | What is part number for the front display module (FDM) Masterpact electronic-trip breakers. The Front Display Module (FDM) catalog number is TRV00121. |
| FA22772 | What is the difference between 31088 and 31097 key locking devices. 31097 keylocking device is used for the Single Handle Source Changeover Assembly in which different type off cam is used. These cams are to be ordered... |
| FA12076 | How to connect the Altistart 48 to motor delta terminal with existing star delta starter as bypass arrangement. The Circuit diagram of Altistart 48 connection to motor delta terminals with existing star-delta starter as bypass arrangement is attached. |
| FA22631 | What is the reference of Type A or Type B thermostat in Prisma Plus switchboard. Type C thermostat is available in Prisma Plus, the part reference of which is 08998. The Type C thermostat Reference 08998 can be used as Type A or... |