Options and Accessories - FAQs

FAQ Search
Most Recently Published FAQs

Results 81 - 90 of 100

FAQ ID Description
FA172159What is the part code for a lead for XS618B1PAM12?
 The code is XZCPV1141L2 for a straight plug with 2m PVC lead The XZCPV1241L2 is an angled plug with 2m PVC lead Longer lengths may be available,...
FA172188What code is an enclosure suitable for an Emergency stop?
XALK01 is a single 22mm hole enclosure with a light grey base and yellow lid. XALK01H29 is the same but also has Emergency Stop engraved on the lid....
FA172195What is the part code if I need a ZB4BG2 key switch, but with a different key then the standard 455 key?
One option is a ZB4BG212. This has a 421E key.
FA172201What code is a light block for the XALD or XALK enclosures?
Depending on the voltage and colour required the codes are ZALVB* for 24vAC/DC, ZALVG* for 48-120vAC or ZALVM* for 230vAC
FA237150What is the difference between BMXRMS008MPF and BMXRMS008MP.
There is a difference of memory size between the two.  BMXRMS008MP can store 8MB data.  BMXRMS008MPF card that you can use the data file storage...
FA237084Do we have any product in our Phaseo ABL range which shows display and relay output function.
In our Phaseo ABL8 power supply range we have the input & output supply healthy indication LED`s available with auto & manual output selection switch. Similarly...
FA32985What is the difference between a VPIS and a VDS (SM6, RM6 power ON pilot light)?
VPIS (Voltage Presence Indicator System): According to standard IEC 61958 the purpose of a VPIS is to signal a voltage presence. If a lamp is unlit,...
FA23919What are the values of the 1P breaking capacities of GV2P circuit-breakers in IT earthing system?
The values below are the breaking capacities of GV2P circuit-breakers operating on an IT earthing system at 400 V 50 Hz, as demonstrated by pole-by-pole...
FA141655Will Zelio Soft 2 V4.5 work on Windows 7 64 bit?
  Yes, the only current issue that arises is when it comes to communicate between the PC/Laptop and the Zelio Logic Relay, if you use the USB cable...
FA141801Where to get drivers for the Bluetooth adaptor VW3A8115 for Zelio Logic Smart Relay SR2/SR3/Twido/ATV?
The drivers are contained in the CD, included in the Bluetooth adaptor kit accompanies, those drivers are also obtainable here. Bluetooth adaptor...

Results 81 - 90 of 100