| FA170506 | Is it possible to enable "Auto Scrolling" for the EM6400 series meter display. Auto Scroll allows the user to monitor a group of Display Pages sequentially, every 5 seconds, without constant key pressing.
There are three different... |
| FA170008 | How do I use Microsoft Windows Media Player ActiveX in Citect. You will need to set the Media Player ActiveX object property to specify the filename that needs be opened and also call the Play Method via Cicode:
1.... |
| FA170007 | Can I zoom window while drawing objects in graphics builder. Yes, use the Zoom command to view an enlarged view of your drawing. The Zoom command displays a zoom box on screen that
magnifies the area around... |
| FA170006 | What is the idle logout time of Vijeo Citect logged-in user. The user will not automatically logged out bydefault , either you need to call Logout() function or need to configure LogoutIdle() function
which... |
| FA12064 | How to change page resolution in configured project of Vijeo Citect. S In order to change the resolution of the pages in Vijeo Citect project do following things: 1. Add the following INI parameter through... |
| FA168469 | How can I change a INI parameter during Citect Runtime. You can update a INI parameter with help of the function “ParameterPut”. This function updates a system parameter in the CITECT.INI file.
If the... |
| FA168468 | How can I configure Menu in the tab style template. Page menus in the tab style templates are defined using the Menu Configuration dialog. For tab templates the fields have the following properties:
Order
The... |
| FA168466 | We frequently need to view the Trends from the trends backup files inside the Vijeo Citect project. The backup files are the trends files moved from the trend folder into a backup folder. To view trend data in Vijeo Citect runtime, you need to add the trend files in Citect with help of the " TrnAddHistory " function available .
Details... |
| FA168463 | How to make factory default the Altivar 312 drive. In the menu drC [Motor Control]:
FCS [Return to factory defaults] :Ini
Press ENT button on the HMI for 2 seconds until NO appears on... |
| FA168462 | How we can run Altivar 312 drive without motor load. Configure following parameter
FLt (Fault menu) OPL (Output phase loss)= NO.
By setting above parameter, you can check drive without physical connection... |