| FA12094 | How to convert DINT variable to REAL variable in Concept (with IEC disabled). In order to convert DINT variable to REAL variable in Concept (with IEC disabled) make use of EMTH-CNVIF instruction. |
| FA12098 | Where is the location of the Elementary Function Block (EFB) library in concept V2.6. EFB library gets loaded automatically when Concept is installed and is available at the location x:\Concept\Lib.Where, 'x' is the root directory. |
| FA12099 | What is the accuracy of the Premium PLC CPU real time clock. Real time clock accuracy:Accuracy of the real time clock is one second (%SW50) +/- 200ms.Resolution of the real time clock is one second (%SW50) +/-... |
| FA12114 | How can we set the time and date in Modicon PL7 Premium CPU. The procedure for setting the time and date in Modicon PL7 Premium CPU is as follows: 1. Open the PL7 Pro project. 2. Make a configuration by selecting... |
| FA86518 | How to resolve the problem of program retention for Quantum Processor on power recycle The problem of program not retaining in the Quantum Processor on power recycle even when the battery is healthy is mainly due to the user application... |
| FA134937 | What would be the maximum timer preset value in Quantum. The maximum timer preset value is 4294967.295 seconds |
| FA143567 | What are the Command Bits for the TSXCTY2C in Unity software. The table below shows the Command Bits for the TSXCTY2C counter module when used in a Unity application.
|
| FA159970 | How to do Twido Modbus addressing in TwidoSuite Software. Refer to attached document for complete Twido Modbus addressing in TwidoSuite Software with examples and modbus function codes. |
| FA136531 | How to load application program into Twido Controller using multifunction USB cable TSXPCX3030. Refer to attached resolution illustrating the complete procedure for loading the application program into
Twido Controller using multifunction USB... |
| FA136535 | Provide us the list of AT Commands applicable for GSM Modems SR2MOD02 AND SR2MOD03. GSM Modem SR2MOD02 is pre-configured to be used with SR2/SR3 Zelio Logic Smart Relays with clock function.
GSM Modem SR2MOD03 is pre-configured... |