Narrow By
  1. Your SelectionAll

Settings - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA170506Is it possible to enable "Auto Scrolling" for the EM6400 series meter display.
Auto Scroll allows the user to monitor a group of Display Pages sequentially, every 5 seconds, without constant key pressing.   There are three different...
FA170007Can I zoom window while drawing objects in graphics builder.
Yes, use the Zoom command to view an enlarged view of your drawing. The Zoom command displays a zoom box on screen that magnifies the area around...
FA170006What is the idle logout time of Vijeo Citect logged-in user.
The user will not automatically logged out bydefault , either you need to call Logout() function or need to configure LogoutIdle() function which...
FA170004What is the Vijeo Citect command to get license serial number.
You need to follow the below command in windows command prompt to get the license details
FA12064 How to change page resolution in configured project of Vijeo Citect.
S    In order to change the resolution of the pages in Vijeo Citect project do following things:          1. Add the following INI parameter through...
FA168472What is the default update screen time of Vijeo Citect and how can I change this.
After successful compilation of the Vijeo Citect project when you run computer setup wizard then before completing the wizard  you get this screen...
FA168467Report using Report Development Tool of VJH 4.3 ,The report looks fine when viewed on any of the browsers, but when we use ‘export to PDF’ option, the appearance of the report gets changed.
You need to change the Page Size of the report in Format report . Change the report Width, height will be automatically adjusted according to the...
FA167854How can I make VJC as a OPC Client to get data from an OPC Server.
For communicating VJC with an OPC Server, you have to select OPC in the IO Device configuration. When you run IO Express Wizard, you have to select...
FA167847On Windows Server 2008 platform during the installation of VJH a message appears stating ASP.NET are not installed.
To resolve this you need to change the UAC (User Access Control).  Navigate to Control Panel -> User Accounts -> User Accounts -> "Change User Account...
FA167190How to set the page resolution of a graphic page in VJC.
While creating the new page you can select the page resolution as shown in below : Or if you have to change the page resolution of an existing...

Results 1 - 10 of 100