| FA167186 | How can I navigate to the data folder of Vijeo Citect directly. You can directly navigate to the DATA folder which have defined in computer setup wizard or to the default location
using Citect Explorer >> View... |
| FA167185 | I am not able to open more than 4 windows using super genie in Vijeo Citect. The maximum number of windows that can be open simultaneously is 4 by default.
Using [Page]Windows ini parameter ,You can sets the maximum number... |
| FA167182 | How to start Vijeo Citect ( VJC ) runtime from the project editor. You can start VJC runtime by doing
go to File >> Run(F5) to start runtime from project editor.
Before starting the runtime kindly make it sure that... |
| FA166629 | When I start the control client from a web client the Internet Explorer information bar displays telling me that it has blocked the running of scripts or ActiveX controls. One of the reasons for this issue is Internet Explorer security preventing the download of any ActiveX controls.
To resolve this issue, add the web... |
| FA166406 | How to update the time and date in a Quantum CPU like 140CPU67160. The Date and Time in a Quantum CPU can be defined by the user if %S50 is high.
System words containing date and current time (in BCD):
%SW49:... |
| FA166405 | How to set the Holdup time in STBNIP2311 module.
The output of the STB Island can be maintained for a duration which can be adjusted.
To change the Holdup Time in an STB Island, go to the NIM web... |
| FA166378 | Does OPC driver support Arrays or OPC DA2 (Data Access 2.0) methods. OPC driver V1.07.00 and later supports OPC DA2 methods of connection.
You need to set the following Citect.ini parameter for this to work -
[OPC]UseOPC2=value... |
| FA166331 | What is the procedure for factory setting (default value) parameter in Lexium 32 drive. Program the Parameter FcS- to rStF (Restore factory settings) in Conf (Configuration) Menu.
Refer to attached file for more information.
|
| FA166246 | Why is the Download selection in Vijeo Designer grayed out. The download option is grayed out in Vijeo Designer only when the Vijeo Designer trial version is installed.
You can only download into the HMI... |
| FA166240 | Can we use other loopback addresses in Vijeo Citect SCADA in addition to 127.0.0.1. All the Internet Protocol address from any address in the range 127.0.0.1 to 127.255.255.254 is mapped as loopback ip address.
Loopback address is... |