| FA145949 | How can I view the HMI screens developed in Vijeo Designer on a Vijeo Citect operator station. We can look the Vijeo designer screens in Citect SCADA with the help of Web Gate features. You have to use the Web Gate
Active X which you can select... |
| FA142634 | How many numbers of objects we can assign on each page. The limitation of Animation object per page is 32000. |
| FA142632 | How to configure the logout option from Citect`s runtime screen when the system is idle for some time. There is LogoutIdle() parameter available in Citect`s INI file. If the current user does not execute any command
within the specified idle time,... |
| FA142633 | What would be the addressing syntax to read Modbus registers from different address locations with Modnet driver. To read input registers from different locations from a device with modnet driver, we suggest you to put "G" prefix
in front of the variable address... |
| FA142630 | How to configure password expiry period in Vijeo Citect. For configuring the password expiry period ,you use a INI parameter i.e. [General]PasswordExpiry.
It determines how long your user and operator passwords... |
| FA141230 | Can we write to any Modbus Device through Vijeo Citect SCADA which does not Support Function Code 06 (Preset Single Register) but Support Function Code 16(Preset Multiple Register) By default Vijeo Citect uses Function Code 06(Preset Single Register) and Function Code 16 (Preset Multiple Register) depending
upon the method to... |
| FA141234 | What is the function of Server Password that is available in Server Authentication Section in Vijeo Citect Computer Setup Wizard. The Server Password is a token key for the server which is required by server and client which is
required to access the CtAPI Server.This password... |
| FA141236 | In Vijeo Citect can Server and Client be of different version. Yes while configuring the Server Client architecture it is possible to have Sever and Client of different version.
It is recommended to have the Server... |
| FA141235 | How to enable Global Event and user defined Event in Vijeo Citect. Events can be enable from Events Setup section of Citect Computer Setup Wizard.
To enable the global events check the option ‘Enable Events on this... |
| FA141078 | How can I know license point counts that my project is using. There is not such option to count the exact point being used in citect project because the point counts
varies depending upon the architecture of... |