| FA136033 | How to program the Altivar 71 drive for the reference by modbus and command by logic input LI1. Below is the programming parameter setting for the Reference by Modbus and command by LI1:-
Fr1 => [Modbus] (Mdb)
CHCF => [Separate] (SEP)
... |
| FA136031 | Is it possible to maintain the some speed, if the modbus cable is disconnected or broken from the Altivar 71 drive. Yes, it is possible to maintain the some speed by the drive in case of the modbus cable is disconnected
or broken by below setting.
Program SLL... |
| FA134631 | What is the default IP Address of the Modicon M258 controlller. When Modicon M258 controller is straight out of the packaging box, the default IP address is
10.10.x.y (Where x and y are the last two places from... |
| FA12144 | How to connect external potentiometer in Altivar 31 drive. You have to program the parameter Frequency Reference 1(Fr1) = AI1 in Control menu (CtL) for potentiometer. Refer to the attached file for potentiometer... |
| FA27930 | How can I create and modify a password in a ZELIO LOGIC SR2 and SR3? Entering the password
Go to: CONFIGURATION menu, PASSWORD section
Initially, the key is not displayed and each digit is set to 0. The message ENTER... |
| FA22735 | I don't like the tone of the audible module (buzzer) of the XVPC signal towers. Do you have other versions? The audible signaling units (buzzers) on XVPC signal towers are supplied with the option to choose one of 10 tones.
Method for changing the factory-set... |
| FA22711 | What mounting tips can you give for single beam polarised reflex type detectors with the mute function connected to an XPSCM11 Summary of the mute function of an XPSCM Preventa module:
The Preventa XPSCM module mute mechanism allows materials to be transported across the... |
| FA22710 | What mounting tips can you give for single beam proximity detectors with the muting function connected to an XPSCM1144? Summary of the muting function of an XPSCM Preventa module:
The XPSCM Preventa module muting mechanism allows materials to be transported across... |
| FA22654 | What is the significance of two arrows on the knob of Tesys GV3P Current Setting Dial. The first black arrow needs to be set at the rated current of Motor, when Tesys GV3 MPCB is used with contactor separately mounted or not used at... |
| FA142349 | Do we have any retrofit accessory that converts extended rotary handle GV2AP01 to GV2APN01. The GV2APN01 is the extended rotary handle for GV2P/L series of MPCB. The GVAPP1 is the retrofit accessory that
converts GV2AP01 to GV2APN01.
|