Narrow By
  1. Your SelectionAll

Standards - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 33

FAQ ID Description
FA12081What is the Life Cycle Assessment (LCA) for the Multi9 product range.
For Multi9 product ranges, Mean Time To Failure (MTTF) values is used for assessment of the product life cycle. MTTF is the estimated reliability...
FA166323Are the EasyPact CVS circuit breakers in compliance to the tests for electromagnetic or mechanical vibrations.
EasyPact CVS devices resist electromagnetic or mechanical vibrations. Tests are carried out in compliance with standard IEC 60068-2-6 for the levels...
FA166310What are the international standards to which EasyPact circuit breakers are in compliance for Climatic withstand tests .
The EasyPact CVS circuit breakers are in compliance with the tests defined by the following standards for extreme atmospheric conditions:   ...
FA166309What is the pollution degree for EasyPact CVS circuit breakers.
EasyPact CVS circuit breakers are certified for operation in pollution-degree III environments as defined by IEC standards 60947-1 and 60664-1 (industrial...
FA166308What is the degree of protection for EasyPact CVS circuit breakers.
The following indications are in accordance with standards IEC 60529 (IP degree of protection) and IEC 62262 (IK protection against external mechanical...
FA143272Which Analog modules from Premium family support HART protocol.
We have no analog  Premium module  working  with HART protocol.
FA12038What is the naming convention for Vijeo Designer application.
The following characters are valid characters that can be used for naming parts, devices, object, variables and passwords in Vijeo-Designer. a) Alphabet...
FA12141What is the heat dissipation of the Altivar 61 Drive when it is in Ready state.
The heat dissipation value of the Altivar 61 Drives when in Ready State (RDY - Drive is powered up but motor is not running) depends on the size of...
FA12119What is the minimum recommended Ground to Input Phase insulation resistance for Altivar 71 Drive.
The Insulation resistance value between Ground to Input Phase should be greater than 1 Mega Ohms which is the Megger value at 500 V for 1 minute.
FA23926What is the meaning of the utilization categories AC1 and AC3 for the Tesys contactors?
The standard utilization categories defines the current making and breaking values for contactors. They depend on the following: The type of...

Results 1 - 10 of 33