| FA170718 | In a linear load application, is IT earthing acceptable to use AC type C60 Vigi module. For IT earthing system must use ASi or ASiE devices to avoid nuisance tripping of C60 Vigi modules.
The main reason is due to Neutral line is not... |
| FA170716 | Is it necessary to connect the Acti9 range of contactor (iACT24) to the 230VAC power supply. The 24VDC is just used to send the command, from Acti 9 Smartlink or a PLC. To be able to energize the coil of the
associated contactor, the iACT24... |
| FA170714 | What is maximum length of the cable between MCB and Acti9 Smartlink. The cable length between an input of the Acti9 Smartlink and any device connected is limited to 20 meters. |
| FA170712 | What's the burden of BCPM power consumption. The BCPM is fused at 500mA so, that will be the absolute maximum it could draw, however we expect normal draw to be less than 100mA.
So if the... |
| FA170616 | Is it possible to operate or configure ATV303 drive with remote HMI
Yes, it is possible to operate and / or to configure ATV303 drive by means of remote HMI Part reference VW3A1006.
|
| FA170610 | When Lexium 32 range of servo drive goes into the “QUICK STOP”. Lexium 32 range of servo drive goes into the QUICK STOP under two conditions
If servo drive meet with an error of class 1 or class 2.
Upon... |
| FA170609 | In Lexium range drive the permissible range of motor shaft movement if absolute position is to be retained while servo drive is powered off. Permissible range of motor shaft movement is +/ - 0.25 revolution from the position at which motor shaft position was
at the moment servo drive was... |
| FA170608 | In Altivar range of drives ,display of current (A) is blinking on 7 –segment LED display. What does this mean. Blinking of Current (A) displayed on 7-segment LED display indicates that drive has reached to the current limitation.
This occurs when current drawn... |
| FA170509 | Where is the Test Button resistor connected between the poles of Vigi iC60 devices (3P and 4P). The Test Button resistor is connected between the poles 2 and 3 of Vigi iC60 devices (3P and 4P).
Please refer the below diagram
|
| FA170508 | What is the earth fault loop impedance values (Zs) for the Acti9 iC60 MCB’s. The earth fault loop impedance values for Acti9 iC60 are given in below table.
|