| FA171254 | What kind of Technology is used in Type 1 and Type 2 class of surge arresters. The Type 1 (PRF1 surge arresters) use “encapsulated air-filled spark gap “ type technology without arc device while as the
Type 2 (PRD surge arresters)... |
| FA171253 | Are Multi 9 and Acti 9 contactors CT/iCT in compliance with the EN 61095 standard. Our Acti9 and Multi9 range iCT/CT are fully compliant with EN61095.
The EN61095 is the dedicated standard for contactors for household and similar... |
| FA171252 | What is the classification of Acti 9 range of products for Corrosive atmospheres. For Corrosive atmospheres the classification is 3C2 (urban regions with industrial activities, heavy traffic) as per IEC 60721-3-3 for
Acti 9 range... |
| FA171250 | What is the Dielectric resistance of Acti 9 smartlink prefabricated cables. The Dielectric resistance of Acti 9 smartlink prefabricated cables is1kV/5min. |
| FA171076 | Would digital inputs of LXM32 servo range drives take effect when SoMoveLite control panel access is enabled. When SoMoveLite control panel access is enabled, it is exclusive control and will be given top priority. So, effect
of activating digital inputs physically... |
| FA171072 | What is the difference between pre-cabled connectors (1) XZ CP1141L2 and (2) XZ CP1169L2 when both are 4 pins, female, straight and M12 connectors. Difference between (1) XZ CP1141L2 and (2) XZ CP1169L2 is as below.
==> XZCP1141L2 is a straight, 4 pins M12 Female connector with PUR cable of... |
| FA170718 | In a linear load application, is IT earthing acceptable to use AC type C60 Vigi module. For IT earthing system must use ASi or ASiE devices to avoid nuisance tripping of C60 Vigi modules.
The main reason is due to Neutral line is not... |
| FA170716 | Is it necessary to connect the Acti9 range of contactor (iACT24) to the 230VAC power supply. The 24VDC is just used to send the command, from Acti 9 Smartlink or a PLC. To be able to energize the coil of the
associated contactor, the iACT24... |
| FA170714 | What is maximum length of the cable between MCB and Acti9 Smartlink. The cable length between an input of the Acti9 Smartlink and any device connected is limited to 20 meters. |
| FA170712 | What's the burden of BCPM power consumption. The BCPM is fused at 500mA so, that will be the absolute maximum it could draw, however we expect normal draw to be less than 100mA.
So if the... |