| FA169755 | What is the default baud rate , address and parity of Breaker Communications Module (BCM) and Chassis Communications Module (CCM). For the CCM the Default values are: Baud rate = 19.2 K , Address = 97, Parity = even
For the BCM the default values are: Baud rate = 19.2 K, Address... |
| FA169752 | Is there any dual redundancy available with TeSys T’s offer. Yes, it is available with Ethernet Product only. This is the dual port technology which allows that.
The redundancy is for Ethernet Communication... |
| FA169751 | Is it possible to feed the supply from top (upstream) and bottom (downstream) in compact NSX range MCCB. Compact NSX circuit breakers can be supplied from either the top or the bottom, even when equipped with a Vigi
earth-leakage protection module, without... |
| FA169750 | What is the memory capacity of the processor used on the Micrologic 5 or 6 E trip units. The microcontroller has 512 Kbytes in Flash memory and 32 kBytes in RAM on the Micrologic 5 or 6 trip units. |
| FA169749 | Is it possible to use the 3 poles NSX circuit breakers with 3 pole Vigi module on a single phase application. The Vigi module can be used in a single-phase configuration for a 3P type. The Vigi works in single-phase between two phases,
The test push button... |
| FA169748 | What is the definition of the term OSN on micrologic electronic trip units. OSN (Over Size Neutral) means that the neutral protection is 1.6 times greater than the phase protection.
This type of trip unit is used if there... |
| FA169747 | How to obtain the manufacturing date code of the Compact NS or NSX circuit-breakers from the MCCB. To obtain the manufacturing date of Compact NS or NSX circuit-breakers, read the screen-printed marking at the top of the front panel.
For example... |
| FA168471 | How can I look at the compilation errors in Vijeo Citect. When you compile your Vijeo Citect project then a message appears and shows warnings & error messages, if you again want to re-check
those messages... |
| FA168470 | Where did I find the Citect.ini file in my Windows 7 system. The citect.ini files in a Windows 7 System will be found in the given below location.
C:\ProgramData\Schneider Electric\Vijeo Citect 7.20\Config
|
| FA168464 | Does Altivar 212 has options of Ethernet card for communication. Altivar 212 doesnot have Ethernet card as an option. However you can use ethernet gateways for communication devices on Ethernet protocol. |