| FA166983 | What is TSX CRJMD25 Cable. The TSX CUSB 485 converter requires the use of the TSX CRJMD 25 cable (equipped with 1 mini-DIN connector and 1 RJ45 connector).
TSX CUSB 485 + TSX... |
| FA166982 | How to know which HotFix or updates are already installed with Unity Pro installed in your PC. Open Unity Pro, click on “Help”, “about Unity Pro” and “Technical Information”: The list of installed Hot Fixes is displayed.
|
| FA166626 | What is mean by Persisted IO Device and how can I use this in Vijeo Citect V 7.20. With the release of V7.20, a feature called persistence can be applied to I/O devices. When implemented, the tag cache for
an I/O device is written... |
| FA166625 | What is the difference between the “ReportManager” and the “ReportServer” in Vijeo Citect. Report Manager is a convenient web user interface to the Report Server that enables you to view and administer
your reports, data sources, and report resources.
Report Server... |
| FA166623 | What is the difference between TSXPLP01 and TSXPLP101. TSXPLP01 and TSXPLP101 are used for Internal RAM memory backup on TSX P57 processors and fitted in the power supply module.
TSXPLP01 is reference... |
| FA166620 | What is the difference between the 490NAD91103 and 490NAD91104 in a profibus network 490NAD1103 is line terminator used in profibus network where as the 490NAD91104 is in line connector. |
| FA166619 | What is HART Protocol and which module supports HART Protocol. The Highway Addressable Remote Transducer (HART) protocol provides digital communication to microprocessor-based
analog process control instruments.... |
| FA166617 | Are M340 CPU modules are 32 bit processors. Yes,M340 CPU modules are 32 bit processors. The Processor is from ARM9 family a 32 bit RISC (Reduced instruction set computing). |
| FA166616 | Is it possible to establish communication between SoMachine platform PLC and vijeo designer simulator. Yes, it is possible to establish communication between SoMachine platform PLC and Vijeo designer simulator
by using Modbus TCP/IP protocol.Set IP... |
| FA166615 | Can ATS22 Soft-starter be used to operate 2 speed motor. It is possible to operate two speed motor with ATS22
With ATS22, make two sets of Motor rated current (In and In2) , Current limit (ILt and ILt2),... |