Narrow By
  1. Your SelectionAll

Technical Characteristics - FAQs

FAQ Search
Most Recently Published FAQs

Results 61 - 70 of 100

FAQ ID Description
FA166613How to operate ATV312 with preset speeds.
Preset speed function can be assigned two ways to Altivar 312. 1) Logic inputs  2) Communication networks   1)Through Logic inputs   To assign preset...
FA166612How KWH reading in ATS48 can be known.
KWH value is not displayed on display of ATS48 but it can be read by connecting product online to Power suite software. With power suite it is available...
FA166611With ATV312,keeps on pressing MODE button during 3 seconds, drive should switch from remote configuration to Local configuration and vice-versa but it is not working. What could be the reason.
 Remote to Local configuration switching and vice-versa by means of pressing MODE button for 3 seconds is made available to ATV312 drive from product...
FA166610Is it necessary to have Lexium CT installed before installing Lexium 32 Flash Tool.
It was must to have Lexium CT installed before installing Lexium 32 Flash tool”setup_flash3_v2.5” but with newer version of Lexium 32 Flash tool”...
FA166609When using ATS22, what is difference between motor overload alarm and motor overload trip (OLF).
When motor thermal state as calculated by starter is reached to 110%, motor overload alarm is triggered but when motor  thermal state continues to...
FA166608When over sized selection of ATS22 is mandatory. How to do oversize selection.
The Altistart 22 rating is limited to 3.5 IcL. IcL is the nominal current of the Altistart 22. If the application requires a higher rated starting...
FA166607What does “tBS” mean in case of ATS22 or ATS48 soft-starter. Does it indicate fault state of soft-starter.
 “tBS” does not indicate any fault state of soft-starter but as it name suggests it is “Time before re-starting”. It can be set in unit of seconds....
FA166606What minimum power of motor could be operated with ATS22 soft starter.
ATS22 is having inbuilt bypass contactor and its switching takes place only when Imotor (Actual Motor current) of In (Motor rated current set with...
FA166604Are Zx-function keys multifunctional.
Normally, Zx function Keys work as navigation keys. They can also be used in a control diagram while developing logic with zeliosoft2. In this configuration,...
FA166565What cables to be used to connect Local PC to SoMachine software.
TCS XCNA MUM3P:This USB cable is suitable for short duration connection like quick updates or retrieving data values.   BMX XCA USBH045: Grounded...

Results 61 - 70 of 100