| FA166499 | What are the factory default settings in DM6000 series. The factory default settings in DM6000 series is as below,
SET Parameter
... |
| FA166497 | Is it possible to use the reference LA9D901 with the reference LADR, LADS2 etc. The LADS2, LADR* and LADT* are time delay auxiliary contact blocks.
Each reference respond to distinct need, however theirs external design are identically.
Hence,... |
| FA166496 | What is the maximum and minimum height of the bracket LA7F901 and LA7F902 used with LC1F range Contactor. Refer below the heights of these brackets:--
> LA7F901: Hmin= 51 mm / Hmax=84 mm
> LA7F902: Hmin= 64 mm / Hmax=106 mm |
| FA166495 | Is it possible to use the auxiliary switch ref. 29450 (OF/SD/SDE) with Compact NSX DC-PV range MCCB. All accessories and auxiliaries of the Compact NSX DC PV breaker are identical to the Compact NSX DC range
and it is also mentioned in the catalog.
So... |
| FA166493 | Is it possible to have an operation Counter in Easypact MVS range ACB. Yes, it is possible to use same Operation Counter of Masterpact NW in Easypact MVS range ACB.
|
| FA166492 | What is the difference between MSU unit & MN undervoltage release of C60 range MCB. MSU is dedicated to monitor power supply voltage and trips RCB in case this voltage turns higher
than values safe for the appliances. MN will trip... |
| FA166491 | Is it possible to use the same auxiliary contact shunt trip of C60 range with C60H RCBO. Yes, it is possible to use the same auxiliary functions as the C60 circuit breaker, to install on the left of the C60H RCBO. |
| FA166490 | What is the tolerance on the nominal voltage for the C60 electrical auxiliaries. As per the IEC 60947-2 standard, the tolerance for the electrical auxiliaries for the LV breakers is 0.85 of minimum Un
and 1.1 of maximum Un.
Example... |
| FA166489 | Is it possible to use the under voltage release and the shunt trip for the C60H circuit breaker at 400 Hz. For MN under voltage release, there is a specific part number ref. 26959 for 400Hz, 115V application.
For MX shunt trip, it does not operate under... |
| FA166488 | Is it possible to use C60 comb-busbar on DC application. Yes, the comb-busbar for C60 range MCB can be used under DC network. And the rated insulation voltage = 500 V
|