Narrow By
  1. Your SelectionAll

Technical Documentation - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA22590What is the selection criterion of Circuit Breakers for the Capacitor bank application.
The selection should be done after derating the Circuit Breaker taking into consideration voltage variation and capacitors tolerances that could increase...
FA22857 What is the pin-out of the RJ45 socket of an ATV31 for connection of Modbus, CanOpen and PowerSuite cables
     The RJ45 socket of the ATV31 can be used for connection to the following networks and accessories:      a PLC via a Modbus bus or via a CANopen...
FA167816What is the part number and datasheet of Remote graphic display terminal for Altivar 71/61 drive.
The part number of Remote graphic display terminal for Altivar 71/61 drive is VW3A1101. Refer to attached file for the datasheet of Remote graphic...
FA167575In Ecodial Advance Calculation, how will I change the application language?
Before starting/launching the Ecodial Advance calculation:   Go to Start Programs Schneider Electric Ecodial Advance Calculation ...
FA166981What is new in Unity Pro Version V7.0.
Please find attached the PDF file which tells what is new in Unity Pro Version V7.0
FA166494Is it possible to use the 4 pole vigi module with the 3 pole Compact NSX MCCB.
Yes, it is possible to connect the 4 pole Vigi module with the 3 Pole Compact NSX MCCB. For fixing the 4 pole Vigi with 3 Pole Compact NSX100 to...
FA166346What is BUF (Braking Unit Fault) in Altivar 71 Drive.
This fault appears only for the drives > 90kW. This fault appears when there is a short-circuit on the output of the braking transistor (desaturation...
FA166345What is the Type1 & Type2 coordination table for Altivar 61 drive range.
Refer to attached file for Type1 & Type2 coordination table.  
FA166343What is OHF (Drive Over Heating Fault) in Altivar 71 drive.
Refer the attached file for details
FA166342What are the different types of Encoder interface cards available & how to install in Altivar 71 drive.
Refer to attached file for different types of Encoder interface cards available & how to install in Altivar 71 drive.

Results 1 - 10 of 100