Narrow By
  1. Your SelectionAll

Technical Documentation - FAQs

FAQ Search
Most Recently Published FAQs

Results 11 - 20 of 100

FAQ ID Description
FA166318What is the Utilisation category of EasyPact CVS circuit breakers.
The Utilisation category of EasyPact CVS circuit breakers is “A”.   The standard IEC 60947-2 defines two utilisation categories, A and B, depending...
FA135168What adapter to be used with XBT G models of HMI to have communication with Modbus Plus.
We need to use XBTZGMBP Modbus plus USB gateway. Refer the attached file for more details.
FA22433What is the broadcast address in terms of Ethernet network.
A broadcast address is an IP address that is used to target all systems on a specific subnet network instead of single hosts.   In other words broadcast...
FA21084How to convert an application developed in ProWorx Plus V1.65 to Concept V2.6 software.
ProWorx Plus is DOS based software. However, the offline databases for ProWorx Plus and ProWorx NxT are identical. The offline database can be opened...
FA22434How to fix the Error "User Interface Kernel (UIK)" in Concept.
The error "User Interface Kernel" (UIK) comes due to failure of reading the desktop file. The desktop file (project name .dsk) which contains screen...
FA21082Which Modbus functions are used for reading/writing multiple data on IO scanning in Modicon Quantum range.
In Modicon Quantum range, I/O scanning works with following Modbus function codes:   FC3 for Reading Multiple 4X registers. FC16 for Writing...
FA21079How to check the health status of CRA module 140CRA93100 in Concept.
Function block STAT can be used under 984LL section in Concept to check the health status of CRA module 140CRA93100. It will give the communication...
FA138274How to connect terminal box TSXPACC01 to TSX Micro controllers.
Refer to attached Instruction manual for illustration of Terminal box TSXPACC01 connection to Modicon TSX Micro controllers.
FA21072What is the part number of battery (with connector cable) for Modicon Micro range PLC 110CPU31102.
The part reference of the battery for Modicon Micro range PLCs are as follows: Lithium battery assembly 110XCP98000. Battery capacitor assembly...
FA86517What is the life of the Premium Processor battery TSXPLP01
The table below shows the life of TSXPLP01 battery used in Premium range of processors, even if the power is completely off. ...

Results 11 - 20 of 100