Narrow By
  1. Your SelectionAll

Technical Documentation - FAQs

FAQ Search
Most Recently Published FAQs

Results 41 - 50 of 100

FAQ ID Description
FA86625What is the accuracy of the current displayed on HMI (Graphic Keypad) of Altivar 71
The current displayed is an estimation of the effective motor current from phase current measurements that is the current that is measured by the...
FA86623How to switch ACC (Acceleration) & dEC (Deceleration) to AC2 (Acceleration 2) & dE2 (Deceleration 2) in Altivar 71
In order to switch from ACC & dEC to AC2 & dE2, configure rPS (Ramp switch ass.) in [1.7 APPLICATION FUNCT.] Menu to Logic input (LI). For Example...
FA86567Is Current Limit function available in Altivar 21 Drive
The Current Limit function is available in Altivar 21 Drive. The parameter number is F601. The Current Limit range is 10-110% of drive's rated current....
FA86556Why is the Input Current of Altivar 71 HD90N4 to HC50N4 range of drives less than the Output Current
The Input Current of Altivar 71 HD90N4 to HC50N4 range of drives is less than the output current because of the presence of the DC Choke (Lw).   The...
FA86570What is the accuracy of the displayed motor current on the Graphic Keypad of the Altivar 21 Drive
The accuracy of the displayed motor current on the Graphic Keypad of the Altivar 21 drive is approximately +/-10%.
FA86523What is the maximum switching cycle of power permitted for Altivar71
The maximum number of times the power of the Altivar71 that is permitted to be switched is 1 cycle every minute. If the switching cycle is more in...
FA146153How to change the Node name of M258 controller from USB memory stick.
Below are the steps to change the name of M258 controller from USB memory stick.   1) SoMachine Menu Online /USB mass storage include command SetNodename...
FA146152How to upgrade the firmware of ATV-IMC without using SoMachine.
Find attached the description of a tool which allows the user to upload the ATV-IMC firmware in a very simple way, without the use of SoMachine.
FA141466How to upgrade firmware version of M238 Controller.
Refer to attached file for procedure to upgrade the firmware version of Modicon M238 Controller.
FA134991What are the faults that can be reset with the automatic restart function, after the cause has disappeared on Altivar 71 and Altivar 61 drives.
Refer the attached list of the faults which can be reset with the automatic restart function.

Results 41 - 50 of 100