| FA22636 | Is the Canalis range of products KBA, KBB, KDP halogen free. Yes, the Canalis range of products KBA, KBB and KDP are halogen free.
The Declaration of Conformity is attached. |
| FA23936 | What stainless steel accessories are available for emergency stop cable pull switches? The only stainless steel accessories available for emergency stop cable pull switches are the pulley, part number XYCZ708 (X6CR17 ferritic stainless... |
| FA23926 | What is the meaning of the utilization categories AC1 and AC3 for the Tesys contactors? The standard utilization categories defines the current making and breaking values for contactors.
They depend on the following:
The type of... |
| FA22942 | Where can I find the characteristics of the LC1D contactors? You will find all the characteristics of LC1Dxx contactors on the Tesys web page:
The section Downloads has documents ( Catalogues, Brochures, Catalogue... |
| FA22658 | What are the main DC power supply voltage and current ratings of LC1F115 & LC1F150 Contactors. The LC1D115/150 was launched in 1996 in order to substitute the LC1F115/150 in the future, and offer better performances using an improved design.
For... |
| FA137294 | How to connect a 2-Wire sensor to Zelio Logic SR3B261FU. Refer to attached file for a document illustrating connection of 2-Wire sensor to a Zelio Logic SR3B261FU.
The input impedence to be used is around... |
| FA22907 | How does a photoelectric detector operate in "thru-beam" mode? A thru beam sensor uses an external beam transmitter to a receiver that detects when the beam is broken.
Note the following operating precautions:
This... |
| FA22746 | How is content level detected in a transparent bottle by a photoelectric sensor? Sensor number XUMW1KSNLT is a thru beam sensor for the detection of liquid levels in glass and plastic containers. See attached pdf
Though not a... |
| FA162260 | Is there any cascading and coordination table available for Easypact CVS MCCB. Please refer the below file for cascading and coordination charts of Easypact CVS MCCB. |
| FA149426 | How to compile SoMachine Errors due to use of 'VAR PERSISTENT' with 'AT Declaration'. In order to compile SoMachine Errors due to use of 'VAR PERSISTENT' with 'AT Declaration',user should not use the
"AT Declaration" in combination... |