Narrow By
  1. Your SelectionAll

Technical Documentation - FAQs

FAQ Search
Most Recently Published FAQs

Results 71 - 80 of 100

FAQ ID Description
FA22617What is the maximum rated AC current at AC voltage for the auxiliary contacts of C60.
The maximum rated AC Voltage and AC Current for the Category AC12 (IEC 60947-5) auxiliary contacts OF, SD, OF+SD/OF, OF.S (Reference - 26924, 26927,...
FA22614What is the derating table for the Combo Busbar of C60 as per temperature.
Find attached the derating table for the Combo Busbar for C60 as per temperature.  
FA21085Is it possible to configure ring topology with Modbus and Modbus Plus communication networks.
Modbus and Modbus Plus networks support line and star topology only. These networks cannot be configured in ring topology. However, it is possible...
FA22582What is the KA rating of 29372 and 32623 Busbar Adapters for Compact NS/NSX<630 Circuit Breaker.
The breaking capacity (KA rating) of the system with the Busbar Adapters 29372 and 32623 connected with Compact NS/NSX   Derating Table ...
FA22584Why does the display light of Micrologic 6.2 trip unit of Compact NSX not glow even when the load reading is displayed.
Unlike other range of Micrologic the backlighting or display light of Micrologic 6.2 is not self powered by the primary current.   A separate external...
FA22770Is the installation of 31097 locking kit same as the 31088 in Interpact source changeover system.
Yes, the installation of the 31097 & 31088 locking kits is the same, as all key locks have been designed to achieve locking in the OFF position. Refer...
FA22635What is the thickness of the Steel sheet metal of Blokset Panel.
The Steel sheet metal thickness used in Blokset Panel is as per the below table: Blokset Steel sheet metal thickness ...
FA22583What is the full name of the abbreviation 'STR' trip unit.
 The abbreviation 'STR' has a very old origin. The first generations of trip units were called Statimax and 'STR' refers to "Statimax Trip Release".
FA22599What is meant by Thermal image in Compact NSX.
The model representing the conductor heat rise is constructed according to the calculation of a thermal image. It allows the thermal state of the...
FA22655What is the difference between mechanical Interlock EZ2LB0601 & EZ2LB0602 of LC1B Contactor.
EZ2LB0601 comes without bearing & EZ2LB0602 comes with bearing, this is the main difference between these interlocks.   EZ2LB0602 interlock usually...

Results 71 - 80 of 100