| FA170617 | What exactly error E1301 means in Lexium 32 range of servo drives. What precaution need to be taken to overcome it. Error E1301 appears if STO (Safe Torque Function) is not triggered via two redundant inputs STO A and STO B
simultaneously. It means if STO A and... |
| FA170611 | Does “dIS” on display of lexium servo drive indicates fault. How to overcome it. “dIS” on display does not indicate fault state of lexium servo drive but it is one of the states of servo drive.
dIS stands for Switch ON Disabled.... |
| FA170013 | After running for a few seconds, Data Service will automatically stop without any prompts. Backfill can cause the symptom. If "ToTime" attribute is earlier than "FromTime" attribute in a backfill record. Data service will consider it as... |
| FA168240 | What is the meaning of Err 7 in Altivar 58. Err 7 is a Time out error, the display has sent a request to the control board and does not receive answer
It indicates a defect of communication... |
| FA167847 | On Windows Server 2008 platform during the installation of VJH a message appears stating ASP.NET are not installed. To resolve this you need to change the UAC (User Access Control).
Navigate to Control Panel -> User Accounts -> User Accounts -> "Change User Account... |
| FA167845 | Error message when trying to install Vijeo Historian "There was a problem installing SQL Server 2008 R2. Do you want to continue with Vijeo Historian installation". This error is related to the "SA" password supplied during the historian installation. To avoid this please ensure that the "SA" password
entered... |
| FA167815 | Error ' C++ Debug Assertion Failed!' when attempting to send or save DCF files for ION meters within ION Setup. Cause:-
There are two possible causes for this error:
1. The ION Setup installation was not performed by The Administrator login and UAC is enabled.... |
| FA167814 | "Unknown User" error while logging into ION Setup 3.0.
Cause:-
The customer has an older version of ION Setup already installed on the machine and the two versions are conflicting.
Resolution :
Make... |
| FA166628 | When I try to run the Web Client component for the first time, I get a "System Settings Change" message instructing me to restart my computer. What can I do with this. This message appears on computers that contain old versions of some system files necessary by the Web Client Control.
If these files are used by... |
| FA166627 | What is meant by error “No server of type on cluster” while compiling the project. This error means there is no server of the necessary type configured on the server, like you have configured an alarm tag
and you have not defined... |