Narrow By
  1. Your SelectionAll

Options and Accessories - FAQs

FAQ Search
Most Recently Published FAQs

Results 11 - 20 of 100

FAQ ID Description
FA11881What is the part number of the cable used for communication between TSXSCP114 PCMCIA card and other RS485 device.
TSXSCPCM4030 cable is required from TSXSCP114 PCMCIA card to the Modbus branching device TSXSCA50 for connecting other RS485 device on the Modbus...
FA12018What are the functions of the PCMCIA Card batteries, TSXBATM02 and TSXBATM03.
TSXBATM02 battery provides the necessary power backup to save the content of the RAM PCMCIA when the PCMCIA Card is out of the PLC or when the PLC...
FA22674How to disable Windows Task Manager and Ctrl+Alt+Del control from Windows registry.
To disable Windows Task Manager and Ctrl+Alt+Del control from Windows registry follow the below steps :   Click Start Click Run Enter...
FA21083What is the insulation voltage rating for cables BMX FTW and BMX FCW in Modicon M340 range.
The dielectric withstanding (VDC) for cables BMX FTW and BMX FCW is 1000 Volts applied for 1 minute and th minimum specific insulation resistance...
FA22666What are the part reference for the Magelis XBT GT series CF card.
The part reference for the Magelis XBT GT series CF cards are as tabulated below : Memory Size Part Reference ...
FA114Which are the compatible printers that can be configured with Magelis XBT GT terminals.
The list of compatible printers with Magelis XBT GT terminals are as follows:Target Connection with - USB, LPR, IPPa) HP PCL3 (HP PhotoSmart, HP DeskJet...
FA86681Which are the Encoder Option cards available for Altivar 71 along with their part numbers and specification
Six types of encoder cards are available depending on the Encoder Technology (Incremental or Absolute). 1.) RS 422 compatible differential outputs. 2.)...
FA86686Is "Output Contactor Control" function available with Altivar 71
The "Output Contactor Control" function is available with Altivar 71.   For programming of this function and details of contactor control, see attached...
FA86641What is the voltage drop with a AC Line Choke and with DC Choke in Altivar 71
The voltage drop with AC Line Choke is about 3% & 5%.   And with DC Choke the voltage drop is about 4% to 6% of the nominal supply voltage.
FA86668How can the Current Harmonics be reduced up to 5% in Altivar 71
With the help of special Passive Filter the Current Harmonics can be reduced up to 5% in Altivar 71 drives (see attached file). The association of...

Results 11 - 20 of 100