Narrow By
  1. Your SelectionAll

Options and Accessories - FAQs

FAQ Search
Most Recently Published FAQs

Results 31 - 40 of 100

FAQ ID Description
FA28095What are the part numbers of the BA9S type bulbs for XB4/XB5 pushbutton controls?
For Harmony XB4/XB5 22 diameter control and signalling units, whether: LED lamps, incandescent lamps, neon lamps, there are part numbers with BA9s...
FA24940Do the GS1 or GS2 disconnect switches come with fuses?
No, because the fuse is linked to the application, eg:  fast-acting semi-conductor fuses for electronic loads aM fuses for motor loads ...
FA23920What is the operation of the GV2AD fault signalling contacts of the GV2 circuit-breakers?
GV2ME, GV2P, GV2L, GV2LE, GV3P and GV3L circuit-breakers can be fitted with the following optional fault indicating contact blocks:   GVAD0110 GVAD0101...
FA23663What are the part numbers of the replacement contact sets for LC1F power contactors?
Spare parts required for each pole of LC1Fxx contactors are as follows:   2 fixed contacts 1 moving contact 2 deflectors 1 backplate ...
FA23278In what type of control station can I install control and signaling units from the Harmony style 5 range?
Harmony style 5 range (XB5) buttons can be used on the front panel of the following control stations: XALK, XALD: plastic control stations, ...
FA23212Is "remote reset" function available for GV2 / GV3 / GV7 circuit breakers?
No remote reset  is available for GV2/GV3/GV7 circuit breakers. Remote tripping, using shunt trips, is available but no reset. Remote resets are...
FA22942Where can I find the characteristics of the LC1D contactors?
You will find all the characteristics of LC1Dxx contactors on the Tesys web page:   The section Downloads has documents ( Catalogues, Brochures, Catalogue...
FA23032What is an EVERLINK connection and what are its advantages?
TESYS Everlink contactor   TeSys Everlink is an enhancement to Schneider Electric's motor starter solutions, offering combinations of 2 or 3 products...
FA22954What power supplies should I use to supply light curtains?
Schneider Electric guarantees the correct operation of its light curtains if they are powered with the following modules: ABL8RPS24030: Universal...
FA22755How can I perform the "start test" function on an XUSLA light curtain monitored by an XPSMP configurable module?
Test mode function: This function is neither mandatory nor critical since the XUSLx light curtain has a continuous self-test function (type 4 safety). However,...

Results 31 - 40 of 100