| FA145472 | The MAC ID of the STB NIC2211 is 00 00 54 10 01 02. What is the default IP address. The MAC ID is given in the hexadecimal format. For STB NIC2211 we need to convert this hexadecimal directly to decimal to get the
default IP address.... |
| FA22433 | What is the broadcast address in terms of Ethernet network. A broadcast address is an IP address that is used to target all systems on a specific subnet network instead of single hosts.
In other words broadcast... |
| FA145459 | Is it possible to configure the Quantum Hot standby System without the RIO head 140CRP93200/140CRP93100 while using Unity Pro. The minimum requirement for Hot standy system is to have One power supply, one CPU and RIO head 140CRP93200/140CRP93100.
We can configure the Quantum... |
| FA145466 | While opening Unity Pro it shows “Instance of SecUBS and SecPBS creation failed opening them failed”. Follow below procedures
1- Uninstall the Unity Pro
2- Run the below attached setup of Unity Pro Cleaner
3- Restart the PC/Laptop
4- Re Install the... |
| FA143019 | How to identify in which version of Unity the application is being created or last modified. To identify the version of unity pro application, first open a blank Unity Pro application and then select open option.
Navigate to the project backup... |
| FA145461 | In Unity Pro where IO status bytes are configured for Quantum PLC. Double click the Remote IO Quantum Drop and in the “Config” Tab provide the Starting address of the Status Table and Ending Address of the Status... |
| FA140414 | While importing the variables some of them were assigned duplicate address in unity pro, how can we avoid this. You can avoid this by selecting the option “Overlapping of address generates “as an error.
Go to Tools à Project Settings à General à Management of... |
| FA140415 | How can we increase the number of columns in the ladder logic section of unity pro. You can increase the number of columns by below setting.
Go to Tools--> Project Settings--> Programs--> LD--> Number of column.
Set the number of... |
| FA12115 | How to enable the Navigation Panel option in ProWorx32. To enable the Navigation Panel option in ProWorx32, check the 'Enable Scrolling Navigation Panel' option in the properties window of ProWorx32 Software.Refer... |
| FA22434 | How to fix the Error "User Interface Kernel (UIK)" in Concept. The error "User Interface Kernel" (UIK) comes due to failure of reading the desktop file. The desktop file (project name .dsk) which contains screen... |