| FA12044 | How to establish Magelis XBT GT communication with M340 PLC using USB cable. In order to establish communication of XBT GT Magelis Terminal using standard USB Cable with M340 PLC you have to set the PLC IP to 90.0.0.1 for Modbus... |
| FA12051 | How to backup alarm information to SRAM during runtime in Magelis XBT GT terminal. In Vijeo-Designer, the alarm information (from all 3 types of alarm databases: Active, History and Log) can be backed up to the SRAM so that it is... |
| FA86520 | After downloading project to W@de it is not possible to access via Internet Explorer The most probable reason for the W@de not been able to be accessed via Internet Explorer after downloading project could be due to the http port number... |
| FA145458 | The MAC ID of the TCSEGPA23F14F (Profibus Remote Master module) is 00.80.F4.FF.08.02 what is the default IP address of PRM module. The default IP address syntax of PRM module is 10.10.XXX.YYY
Where XXX and YYY are the last two bytes of MAC address and can be achieved by converting... |
| FA22665 | Is it possible to read the IP address of connected device at runtime in Vijeo Designer. Yes, it is possible to read the IP address of connected devices via scripting during runtime. This feature has been implemented in Vijeo Designer... |
| FA22664 | Is it possible to write a new IP address of connected device at runtime in Vijeo Designer. Yes, it is possible to write a new IP address of connected devices via scripting during runtime. This feature has been implemented in Vijeo Designer... |
| FA140330 | How to enable the option "Include Editor Project" while using HMI STO/STU/GXO model in Vijeo Designer V6.0 You can enable this by below method.
Go to Data location in target properties and select “OPTIONAL DRIVES” as data location. Include Editor Project... |
| FA12038 | What is the naming convention for Vijeo Designer application. The following characters are valid characters that can be used for naming parts, devices, object, variables and passwords in Vijeo-Designer. a) Alphabet... |
| FA140331 | How many logging groups can be made in Vijeo Designer while selecting a variable for the data logging group. For all target types, we can set maximum of 80 data logging groups.
|
| FA117 | How can you configure timer in Magelis XBT GT terminal to turn off the light on the screen. There are different ways available in Vijeo Designer software to control Backlight.1) During Runtime:You can do the required configuration through... |