| FA11565 | How to display Float data type register value of an external device like PLCs at XBT GT terminal screen correctly. To display correctly float data type register value on Magelis XBT GT terminal screen, it is required to make sure to select ‘Low Order First’ option... |
| FA86686 | Is "Output Contactor Control" function available with Altivar 71 The "Output Contactor Control" function is available with Altivar 71.
For programming of this function and details of contactor control, see attached... |
| FA86682 | How to reset the Altivar 71 Drive fault when in Terminal Control Mode Logical Input assignment Menu --> Fault Management --> Fault Reset, one can reset the faulted Altivar 71 Drive from the Terminal when in Terminal... |
| FA86626 | How to download the Current Drive Configuration to the Graphic Keypad and Stored Configuration from the Graphic Keypad to the Drive Refer to procedure in attachment to download the Current Drive Configuration to the Graphic Keypad and Stored Configuration from the Graphic Keypad... |
| FA86623 | How to switch ACC (Acceleration) & dEC (Deceleration) to AC2 (Acceleration 2) & dE2 (Deceleration 2) in Altivar 71 In order to switch from ACC & dEC to AC2 & dE2, configure rPS (Ramp switch ass.) in [1.7 APPLICATION FUNCT.] Menu to Logic input (LI).
For Example... |
| FA86567 | Is Current Limit function available in Altivar 21 Drive The Current Limit function is available in Altivar 21 Drive. The parameter number is F601.
The Current Limit range is 10-110% of drive's rated current.... |
| FA86570 | What is the accuracy of the displayed motor current on the Graphic Keypad of the Altivar 21 Drive The accuracy of the displayed motor current on the Graphic Keypad of the Altivar 21 drive is approximately +/-10%. |
| FA86576 | Is it possible to use 3 different control channels 1) Comm. 2) HMI (Graphic Keypad) 3) Terminal for controlling the Altivar 71 The 3 different control channels 1) Communication 2) HMI (Graphic Keypad) and 3) Terminal for controlling the Altivar 71 Drive can be achieved by... |
| FA86523 | What is the maximum switching cycle of power permitted for Altivar71 The maximum number of times the power of the Altivar71 that is permitted to be switched is 1 cycle every minute. If the switching cycle is more in... |
| FA146154 | How to Upload or Download files to M258 Controller with USB Memory Key. The Modicon M258 Logic Controller allows file transfers with a USB memory key. Using this USB Memory key,it is
not necessary to use SoMachine or... |