Narrow By
  1. Your SelectionAll

Technical Characteristics - FAQs

FAQ Search
Most Recently Published FAQs

Results 11 - 20 of 100

FAQ ID Description
FA170507How many stop bits does the EGX support.
All EGX devices use an 11-bit frame serial frame. 1 start-bit, 8 data-bits, and 1 or 2 stop bits depending on the parity selection.   Even parity:...
FA22590What is the selection criterion of Circuit Breakers for the Capacitor bank application.
The selection should be done after derating the Circuit Breaker taking into consideration voltage variation and capacitors tolerances that could increase...
FA170012What is difference between floating point and static point licensing in Vijeo Citect.
A client license can be static or floating depending on requirements Static client license: For operators needing access to the system at all times,...
FA170011How to exit the vijeo citect from demo mode.
When you start Vijeo Citect runtime it will check for the license key and if did not found any valid license then automatically starts in demo mode....
FA170003What are the changes in client licenses for Vijeo Citect V7.30.
With the release of new Vijeo Citect V7.30 the distinction between Web and non-Web client versions has been removed. The difference between the Control...
FA169761What does ‘Integr Inst’ means when looking at the trip history on a micrologic P.
The message ‘ Integr Inst' means a tripping by the instantaneous self-protection built into the device that is called as DIN/DINF.  When such message...
FA169760Is there any temperature derating table available for Compact NSX DC PV circuit breaker.
The temperature derating table for Compact NSX DC PV circuit breaker is attached below.
FA169759What is the maximum rated operational voltage (Ue) of Compact NSX DC PV MCCB.
The maximum rated operational voltage of Compact NSX DC PV MCCB is 1000 VDC.
FA169758Is it required to remove the rating plug in Micrologic E of Masterpact NW/NT & Compact NS 630b … 1600 A circuit breakers while performing megger test.
The Micrologic E has a different technology than that of Micrologic A, P and H.   The Micrologic E measures the voltage through a high impedance...
FA169757Is there any tripping curves available for Compact NSX DC PV circuit breaker.
The tripping curves for Compact NSX DC PV MCCB are available and are attached below.

Results 11 - 20 of 100