FAQs

FAQ Search
Most Recently Published FAQs

Results 81 - 90 of 100

FAQ ID Description
FA167841While installing OFS software from VJC installation files , it was asking for Serial Number & part reference.
If you run the OFS installations directly from the installation files then it will ask for Serial Number and Part number, but to install it directly...
FA167822What is the maximum operating temperature & IP of the Remote graphic display terminal of the Altivar 71 Drive.
The maximum operating temperature of the Remote graphic display terminal is 60°C and it has IP 54 Protection.
FA167821What is the benefit of Line Choke for the drive.
Line chokes are used to provide improved protection against over voltages on the line supply and to reduce harmonic distortion of the current produced...
FA167820What is the benefit of Evacuation function on Altivar 71 drive.
This function is suitable for lift application, when there is a power failure; it facilitates the evacuation of people trapped in a lift stuck between...
FA167819What is the Pin out of the Altivar 312 drive RJ45 Connector.
Refer to attached file for the Pin out of the Altivar 312 RJ45 Connector.
FA167817What is the procedure of parameter factory setting for Altivar 71 drive.
Refer to attached file for factory setting of Altivar 71 drive.
FA167816What is the part number and datasheet of Remote graphic display terminal for Altivar 71/61 drive.
The part number of Remote graphic display terminal for Altivar 71/61 drive is VW3A1101. Refer to attached file for the datasheet of Remote graphic...
FA167815Error ' C++ Debug Assertion Failed!' when attempting to send or save DCF files for ION meters within ION Setup.
Cause:-   There are two possible causes for this error:   1. The ION Setup installation was not performed by The Administrator login and UAC is enabled....
FA167814"Unknown User" error while logging into ION Setup 3.0.
Cause:- The customer has an older version of ION Setup already installed on the machine and the two versions are conflicting.   Resolution :  Make...
FA167813Where can I download the lastest firmware revisions for ION and PowerLogic meters.
Below is the Link to download the latest firmware revisions for ION and PowerLogic hardwares.   http://www.powerlogiciframe.com/downloads.cfm/cs/1  

Results 81 - 90 of 100