Narrow By
  1. Your SelectionAll

Options and Accessories - FAQs

FAQ Search
Most Recently Published FAQs

Results 21 - 30 of 100

FAQ ID Description
FA86557How to size the Generator or Transformer required for supplying single unit of Drive
The size of the Generator/Transformer should be 1.5 to 2 times the power in VA to that of the drive that is to be supplied.   Example: The Power rating...
FA86526How to connect the Remote Display (HMI) Unit of Altivar 71 via LU9GC3 Modbus splitter
The Remote Display (HMI) unit of the Altivar 71/ 61 drive takes it power from the drive port to which it is connected. When the same Remote Unit...
FA86530Which Encoder Cards support HTL (High Transistor Logic) signal Encoders for Altivar 71 drive
The High Transistor Logic (HTL) is a type of Push Pull. So VW3A3405 or 06 or 07 Encoder option Board, depending on the excitation power required,...
FA86553Which is the CANOpen address of the register that stores the Encoder Pulse Counts for Altivar 71 drive
The CANOpen address of the register is 201A/5 from where the Encoder Pulse Counts for Altivar 71 drive can be retrieved.
FA23735Where should I connect the SZ1RV1202 potentiometer (pot) to the ATV variable speed drives?
The potentiometer part number: SZ1RV1202 must be connected to one of the 0...10 V analog inputs on ATVxxxx range variable speed drives: ATV12...
FA161909Is it possible to achieve the IP level of the keypad of Altivar 71/61 drive to IP65.
There are additional accessories for the keypad which are remote mounting kit (VM3A1102) and door for remote mounting kit (VW3A1103). With the accessories,...
FA144853What is the purpose of Program Loader TM2USBABDEV1 for Modicon M238 Controllers.
 The TM2USBABDEV1 program loader is an accessory which is designed to simplify updating or duplication of applications on  Modicon M238 logic controllers...
FA144191How many communication ports are inbuilt in Altivar 212 Drive.
Two communication ports are inbuilt in Altivar 212 drive. It enables simultaneous connection to a communication network and an HMI terminal.   Refer...
FA136923What is the meaning of “sold in lots of "(3) VW3A5104 in the Altivar 61 Catalogue – Option: motor chokes (See attachment).
One unit VW3A5104 corresponds to 1 choke for 1 motor phase. That's why Three motor chokes (3 x VW3A5104) are required for three motor phases.
FA12171What is the Part Reference of Resolver card for Altivar 71 Drive.
The Part Reference of Resolver card is VW3A3408.Note: Resolver card VW3A3408 is only compatible with ATV71...383 Drives. This card is not compatible...

Results 21 - 30 of 100