{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Does M580 CPU Support 32-bit processor.

Yes, the M580 ePAC is based on chips that leverage ARM (Advanced RISC Machine) architecture, a family of 32-bit chip sets.

How can I recover a lost password for Unity Pro Application

If you forget your password, proceed as indicated in the following procedures and contact Schneider Electric support. Unity Pro Application Password Schneider Electric support needs a number...

Troubleshooting If Contactor is Humming/Noisy

The video shows different reasons for humming noise and solutions to mitigate the problem. https://schneider-electric.box.com/s/wzg9zl83h6bw6dehpvio1rchcvfzawsz

What is the power consumption value of the Tesys T LTMR controller.

The maximum power consumption of the LTMR (with communication, KE connected, all inputs ON, and all outputs ON) is 9W.

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail

Learn more through our General Knowledge FAQsGeneral Knowledge

How to differentiate power consumption & power dissipation .

The power Consumption in VA is Bus Current * Voltage And the Power dissipation is "lost" or wasted power, represented by the power converted to lower forms such as heat that are no longer...

What is Rated short-time withstand current: Ik (A)?

This is the rms value of the current which the switchgear can carry in the closed position during a specified short time. Short time is generally 1 s, and sometimes 3 s.

What is Rated Transient Recovery Voltage (TRV)?

This is the voltage that appears across the terminals of a circuit breaker pole after the current has been interrupted. The recovery voltage wave form varies according to the real circuit...

We are having issue regarding web deployment, any changes made in SCADA at...

There is an issue in Vijeo Citect v7.20, where the parameter [WebServer]deployRoot does not recognise as a valid value a path enclosed in double quotes. As a workaround, please use an access path...