| FA168466 | We frequently need to view the Trends from the trends backup files inside the Vijeo Citect project. The backup files are the trends files moved from the trend folder into a backup folder. To view trend data in Vijeo Citect runtime, you need to add the trend files in Citect with help of the " TrnAddHistory " function available .
Details... |
| FA168463 | How to make factory default the Altivar 312 drive. In the menu drC [Motor Control]:
FCS [Return to factory defaults] :Ini
Press ENT button on the HMI for 2 seconds until NO appears on... |
| FA168462 | How we can run Altivar 312 drive without motor load. Configure following parameter
FLt (Fault menu) OPL (Output phase loss)= NO.
By setting above parameter, you can check drive without physical connection... |
| FA168244 | What is the use of Automatic adaptation of deceleration ramp parameter on Altivar 312 drive. This function is used to automatically adapt the deceleration ramp if the initial setting is too low for the inertia of the load connected.
It avoids... |
| FA168241 | How to get the Profibus GSD file for Altivar 71/61. Refer to attached file for profibus GSD file of Altivar 71/61. |
| FA167843 | How to set the scaling factor in trends for example if the assign tag (range from 0 - 3600) and show them on trend page automatically. For scaling the trend scale you need to first put the RAW and Engineering scales in the variable tag configuration (snapshot shown below)
with which... |
| FA167817 | What is the procedure of parameter factory setting for Altivar 71 drive. Refer to attached file for factory setting of Altivar 71 drive. |
| FA167810 | How we can set the CT ratios using the button in the front of the ME4zrt device. The CT ratios are settable using the button in the front of the ME4zrt device. You can choose in between
the following for the primary (the secondary... |
| FA167191 | How can I write numeric values in a variable tag of Vijeo Citect. Select a Numeric value ##### from the toolbar and paste it on graphics page. Then right click on it and go to properties.
Then select Input & Keyboard... |
| FA166626 | What is mean by Persisted IO Device and how can I use this in Vijeo Citect V 7.20. With the release of V7.20, a feature called persistence can be applied to I/O devices. When implemented, the tag cache for
an I/O device is written... |