Narrow By
  1. Your SelectionAll

Programming - FAQs

FAQ Search
Most Recently Published FAQs

Results 21 - 30 of 100

FAQ ID Description
FA166618How to sense the plugging and unplugging of Ethernet Cable on TSXETY4103 in Premium Hot standby system.
Define the IODDT for the TSXETY4103 module. Bit CH_ERROR of IODDT T_COM_ETYX103. This becomes 1 when cable is disconnected and zero when cable is...
FA166614What care should be taken if frequency reference from preset speed function is desired but same time analog signal from potentiometer (VDC) is present on analog input (AI1) of ATV312 drive.
While assigning presets speed function, no need to change Fr1 [Ref.1 channel] configuration and it is by default set to AI1 (Analog input AI1).   Preset...
FA166613How to operate ATV312 with preset speeds.
Preset speed function can be assigned two ways to Altivar 312. 1) Logic inputs  2) Communication networks   1)Through Logic inputs   To assign preset...
FA166562What is the behavior of SoMachine when opening *.project of previous version of SoMachine software with newer version of SoMachine software.
When opening *.project of earlier version of SoMachine with newer version of SoMachine software version, message window will appear informing and...
FA166519How "IO profile" is more flexible compare to "DSP-402 profile" in terms of control of Altivar 71/61 drive.
With IO profile configuration, it is possible to have a simultaneous control of drive via The terminals The Modbus control word The...
FA166506Can I restore the OLD setup parameter, while editing the Setup menu in PM1000 Series meter.
Yes, two steps are explained below.   Partially edited set up parameter: While editing the parameter if you want to restore the old set up data press...
FA166500Will the PM1000 and PM1200 Display all three Demand Parameters (A, W & VA) simultaneously.
The PM1000 & PM1200 can read and display only one Demand (A or W or VA) Parameter at a time depending on any one of the parameter which is selected...
FA166499What are the factory default settings in DM6000 series.
The factory default settings in DM6000 series is as below, SET Parameter ...
FA166401How to display counter numeric value on display of zelio smart relay.
Zeliosoft2 configuration software with FBD language contains function block (FB) named “DISPLAY”   Follow below screen shot Connection of Current...
FA166395Give zelio smart relay SR1 to zelio smart relay SR2 correspondence table while transferring zelio-soft V1.5 program running on zelio smart relay SR1 to Zelio smart relay SR2 using zelio-soft V2.0.
While transferring zelio-soft V1.5 application to zelio-soft V2.0 application to make program of zelio smart relay SR1 compatible to run on zelio...

Results 21 - 30 of 100