| FA21084 | How to convert an application developed in ProWorx Plus V1.65 to Concept V2.6 software. ProWorx Plus is DOS based software. However, the offline databases for ProWorx Plus and ProWorx NxT are identical. The offline database can be opened... |
| FA12115 | How to enable the Navigation Panel option in ProWorx32. To enable the Navigation Panel option in ProWorx32, check the 'Enable Scrolling Navigation Panel' option in the properties window of ProWorx32 Software.Refer... |
| FA22434 | How to fix the Error "User Interface Kernel (UIK)" in Concept. The error "User Interface Kernel" (UIK) comes due to failure of reading the desktop file. The desktop file (project name .dsk) which contains screen... |
| FA21082 | Which Modbus functions are used for reading/writing multiple data on IO scanning in Modicon Quantum range.
In Modicon Quantum range, I/O scanning works with following Modbus function codes:
FC3 for Reading Multiple 4X registers.
FC16 for Writing... |
| FA21079 | How to check the health status of CRA module 140CRA93100 in Concept. Function block STAT can be used under 984LL section in Concept to check the health status of CRA module 140CRA93100. It will give the communication... |
| FA12116 | How many devices/registers can be IO scanned by 140CPU65160 Module, Modicon Quantum Range. 140CPU65160 can IO scan up to 128 devices/registers maximum.The total number of input and output words which can be scanned during one cycle is 4000... |
| FA143571 | Is it possible to declare more than 32 input pins to a Concept DFB. No, the maximum allowable input pins on a Concept DFB is 32 |
| FA12094 | How to convert DINT variable to REAL variable in Concept (with IEC disabled). In order to convert DINT variable to REAL variable in Concept (with IEC disabled) make use of EMTH-CNVIF instruction. |
| FA12098 | Where is the location of the Elementary Function Block (EFB) library in concept V2.6. EFB library gets loaded automatically when Concept is installed and is available at the location x:\Concept\Lib.Where, 'x' is the root directory. |
| FA12099 | What is the accuracy of the Premium PLC CPU real time clock. Real time clock accuracy:Accuracy of the real time clock is one second (%SW50) +/- 200ms.Resolution of the real time clock is one second (%SW50) +/-... |