Narrow By
  1. Your SelectionAll

Safety - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 19

FAQ ID Description
FA28005Can I change the contacts on the XCS safety limit switches?
No, it is not possible to change the contacts on XCS limit switches as they are safety devices. There is no replacement part.
FA24894Can I use a "conventional" limit switch for safety applications?
Yes, it is possible to use a "conventional" limit switch for safety applications, as long as the switch is "positive action" Definition of positive...
FA23716Are the XCSDMCx7 coded magnetic switches with contact and LED compatible with the XPSAK or XPSAR Preventa modules?
No, the XCSDMCx7 coded magnetic switches are not compatible, however other Preventa Safety modules are as detailed below: Coded magnetic switches:   ...
FA23690What is the composition of the coded magnetic switches?
The Schneider Electric Coded Magnetic Switch (CMS) is a complete product consisting of two parts: A magnetic switch: this part has a pre wired cable,...
FA22954What power supplies should I use to supply light curtains?
Schneider Electric guarantees the correct operation of its light curtains if they are powered with the following modules: ABL8RPS24030: Universal...
FA22755How can I perform the "start test" function on an XUSLA light curtain monitored by an XPSMP configurable module?
Test mode function: This function is neither mandatory nor critical since the XUSLx light curtain has a continuous self-test function (type 4 safety). However,...
FA22714Dynamic periodic monitoring of dual body valves on an XPSPVK eccentric press
Presses used for cold working of metals must be systematically and regularly checked. This check also affects the safety function provided by the...
FA22719Can the XPE on/off foot switches be used to perform an emergency stop function?
No, as due to their mechanical design, there is nothing to prevent an object from getting under the foot switch and preventing actuation of the contact....
FA22712Simulation of a fault on one of the 2 valve flaps (dynamic monitoring) managed by an XPSPVK
The presses used for the cold working of metals must be routinely and regularly checked. This check also affects the safety function provided by...
FA22711What mounting tips can you give for single beam polarised reflex type detectors with the mute function connected to an XPSCM11
Summary of the mute function of an XPSCM Preventa module: The Preventa XPSCM module mute mechanism allows materials to be transported across the...

Results 1 - 10 of 19