Narrow By
  1. Your SelectionAll

Settings - FAQs

FAQ Search
Most Recently Published FAQs

Results 81 - 90 of 100

FAQ ID Description
FA146153How to change the Node name of M258 controller from USB memory stick.
Below are the steps to change the name of M258 controller from USB memory stick.   1) SoMachine Menu Online /USB mass storage include command SetNodename...
FA145943What is the difference between tLIN and tLIG parameter setting in Altivar 32 drive.
tLIM permit to limit the torque when the motor is in motoring mode and tLIG permit to limit the torque when the motor is in generator mode. So, these...
FA145759What are the parameter settings of Altivar 32 with BSH motor.
 Refer to attached file for parameter settings of Altivar 32 with BSH motor.
FA140831What are the Regular, Periodical inspection & Maintenance points for Altivar 71/Altivar 61 drive.
Refer to attached file for the Regular, Periodical inspection & Maintenance points for Altivar 71/Altivar 61 drive.
FA138760Is it possible to adjust the backlight time of graphic display terminal in Altivar 71.
Yes, It is possible to adjust the backlight time of graphic display terminal in Altivar 71. For this you must set the access level to Expert, then...
FA137616What is the universal password to remove a safety password
The universal password to remove a safety password in Altivar 32 is 1581.
FA137615Is it possible to replace the Telemecanique logo by a specific one in Graphic display terminal (Keypad) of Altivar 71/61.
Yes, it is possible to replace the Telemecanique logo by a specific one in Graphic display terminal of Altivar 71/61.The software is the "Keypad...
FA137613How to reduce noise level of Altivar 71/61 drive which will affect the working of electronic equipment.
To reduce the noise level, do following: - Reduce the switching frequency - Use shielded cables - Separate power cables and control cables
FA136927Why the parameter setting is disappeared automatically, when the power off and on of Altivar 21 drive (with Lonwork card).
According to the LonWorks documentation, the LonWorks card overrides automatically some drive parameters. Refer to attached file.If you modify these...
FA136036What is the minimum motor current to be used with Altistart 22 Soft Starter.
  The minimum motor current value should be 0.4 ICL (nominal Soft Starter current). So, the connected motor current shall not be less then this value...

Results 81 - 90 of 100