Technical FAQs

Ask a Question

What is the difference between LX1 and LX9 coil?

Issue:
LX1 and LX9 characteristic

Product Line:
Tesys F line Contactors and Accessories

Environment:
TeSys™ F AC Coils
 
Resolution:
 The LX1 is the standard control type coil. The LX9 low sealed consumption coil offers high tolerance to inrush voltage drops, immune to micro-breaks (main supply or contact chain) and are capable of operation on networks with harmonic numbers less than or equal to 7.
Was this helpful?
What can we do to improve the information ?