Technical FAQs

Ask a Question

Are replacement parts available for the ATV58 drive?

Issue:
Are replacement parts available for the ATV58 drive?

Product Line:
ATV58, FLEX58

Environment:
All serial numbers

Cause:
Customer has DC bus capacitors leaking or drive is just no longer working properly

Resolution:
This drive is obsolete. There are no longer any replacement parts available for the ATV58. If the drive has stopped working properly, we recommend replacing the drive with a currently-offered drive product.
If the drive is enclosed (such as a FLEX58), then we recommend replacing the entire enclosure rather than just drive. 


 
Was this helpful?
What can we do to improve the information ?