Technical FAQs

Ask a Question

Are the IEC K-Line contactors SEMI F47 compliant?

Product Line:

Tesys K Line Contactors
K-Line contactors are SEMI F47 compliant. Additionally, the addition of an overload relay makes them SEMI F47 compliant motor starters.

The K-Line offering is available in 6 amp and 9 amp versions for SEMI F47 when used with 24 and 120 volt ac control coils. All DC controlled versions are SEMI F47 compliant as standard.

All K-Line products carry the UL, IEC and CE markings. For additional information and other products for SEMA F47 applications refer to the attached link.

Was this helpful?
What can we do to improve the information ?