Technical FAQs

Ask a Question

Will the Tesys GV2ME starters install into old style enclosures designed for the GV2M, GV2MC01 and GV2MC02 enclosures?

Issue:
GV2ME compatibility with old enclosure 

Product Line:

Motor Starters and Protectors

Environment:
TeSys™ GV Manual Starters and Protectors
 
Resolution:
No, Order new enclosures using the same catalog numbers. The current enclosure has an updated DIN attachement which will accept the Tesys GV2ME starters but will not accept the old GV2M starters.
Was this helpful?
What can we do to improve the information ?